Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Serial Communications Driver error on Com1 on boot of the runtime system.
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Serial Communications Driver error on Com1 on boot of the runtime system.
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver-
      • Device Read Error with MicroLogix
      • GESNP / GESNPX 9030 / 9070 Serial Com configuration for Interact / PowerStation PA/PA2/P13 etc...
      • Modbus Device Compatibility with InteractX and Interact Xpress
      • Reading and Writing Allen Bradley Logix tags that are strings
      • Serial Communications Driver error on Com1 on boot of the runtime system.
    • Interact (Legacy)+
    • InteractX+
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Serial Communications Driver error on Com1 on boot of the runtime system.

Print Friendly and PDF

Runtime HMI / PC with InteractX Deployment Server running can block a com port from being used IF the runtime download method selected in the Deployment Server is set to look for "Serial" downloads.

Since the Deployment Server constantly looks for attempts to download updates, the Com port that you pick to do downloads is constantly monitored for a download attempt. This keeps the InteractX COMM Server from using it since Serial ports can not share access like the Ethernet port.

Most units are set to NET for network downloads or NONE if using the USB disk transfer method of updating runtime files.

If you update a unit via USB, it overrides the checked option in the Deployment server and releases the Com port until the unit is rebooted. So, after the USB update, you can run InteractX and there will not be any error since the com port has been freed. On rebooting, the error related to the Com port will show up.

The fix is to only check the serial option if you need to do a serial download for some reason then reset the setting to NONE when the update is complete. The Deployment server icon is in the Windows Desktop System tray.

edited dom 02/13/2019

  • Serial
  • Runtime
  • InteractX
  • Com Error
  • Deployment Server
  • COMM Server
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply