Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
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
  • Motion and Machine Controllers-
    • ACR Controllers+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)-
      • 3rd Party Samples+
      • Embedded Xpress+
      • Errors+
      • Hardware+
      • PAM IDE+
      • Programming Tips+
      • Web Visualization+
      • Quick Start and Online Training Videos
      • Adding New Devices
      • Auto Addressing enabled by default
      • Cam and Gear Program Sample & Video
      • Common PACIO Troubleshooting Tips
      • Compax3 Linear servo motor settings with PAC
      • Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
      • Reading G Code from a file to develop a CNC machine
      • Error: Red triangle on EtherCAT axes/devices when ModBus or ProfiNet connects
      • FTP support
      • How can I send ASCII strings to or from the PAC?
      • How do I configure and gear to the PACIO-454-01 Module?
      • How do I upgrade a Parker Automation Manager (PAM) project from 1.3.0 to 1.4.0?
      • How do I use variables in G code?
      • How to Add ModbusTCP to PAC project (PAC as ModbusTCP slave)
      • How to Set and Get Time / Date / Time Zone Pre-1.4
      • How to Update Devices and their Descriptor files
      • How to Update PAC project without Parker Automation Manager software?
      • How to Update a PAC Firmware? Flashback instructions
      • How to Upload a Program?
      • How to Use the InteractX OPC Quick Client with the PAC
      • How to set up EtherNet/IP Communications with an Allen Bradley PLC
      • How to set Scaling for Parker Mechanics
      • How to use the Outputs on the Compax3-I31 or P series (EtherCAT)
      • IO settings for EtherCAT_Master: How to see IO update while in Stop
      • Log Data to a File
      • Minimum Internet Explorer version for Xpress and Visualization options
      • PAC CNC & Multi-Axis Capabilities, Samples & Video demos
      • PAC CNC visualization
      • PAC System Time Access and Edits
      • PAC Web Visualization with Internet Explorer: missing browser feature HTML5-Canvas Webvisu
      • PAC with .Net or LabView or InteractX: Using OPC DA Server
      • PAC with Modbus: What addresses for tags?
      • Reading Torque from Pseries drive
      • Remanent Variables: Retain vs Persistent Retain
      • Retentive Memory details
      • SDO Read / Write PAC to/from Compax3 I31
      • SMC_ERROR.SMC_FB_WASNT_CALLED_DURING_MOTION
      • Sample Continuous Function Chart CFC Program: time based counter
      • Sample Continuous Function Chart CFC Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Time based counter
      • Sample SFC Program: time based counter
      • Sample Stuctured Text ST Program: Time Based Counter
      • Sample Structured Text ST Program: Basic Motion (Power, Home, Cycle)
      • Single Axis Sample Program with Visualization
      • Two Axis Sample Program with Visualization
      • Using the PAC as a Modbus TCP Master Device
      • Using the PAC as a Modbus TCP Slave Device
      • VIDEO: Run an AC30V an AC Induction motor via EtherCAT with a PAC
      • VIDEO: PAC with Compax3 EtherCAT part 1: EtherCAT connections & Device Selection
      • VIDEO: PAC with Compax3 EtherCAT part 2: Complete Configuration
      • VIDEO: PAC with Compax3 EtherCAT part 3: Setting EtherCAT Master and DS402 scaling
      • VIDEO: PAC with Compax3 EtherCAT part 4: Download & Test in C3 ServoManager
      • Video: Parker's PAC, the Automation Controller Based on IEC61131-3
      • What's the 16# in the axis scaling default of 16#10000?
      • Working with recipes in the PAC
      • Does the PAC have a first scan flag?
      • Error when switching Active Application
      • Using tappets during cam motion
      • WebVisualization not working in PAC terminal (PTA)
      • Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
      • Does PAC act as a OPC-UA server or client, or both?
      • How do I upgrade the PAC from OPC-DA to OPC-UA?
      • How do I use OPC-UA with the PAC?
      • PACIO-441-01 analog current input module
      • Sample code for PACIO-442-02 and PACIO-441-02 analog modules
      • What ports get used with PAC Ethernet connections?
      • C0032: Cannot convert type 'Unknown type: 'ADR(Device.Application.PLC_PRG.x)' to type 'POINTER TO BOOL'
      • CSV Reader Library for the PAC
      • Do I have to upgrade my PAC 1.3.0 Firmware to work with a PAM 1.4.0 project?
      • eCL Homing notes with PAC via EtherCAT
      • EtherCAT communication between the PAC and AC30 drive
      • How to add images to a visualization in WebVis
      • How to reset the EtherCAT bus
      • PAC Terminal Discontinued - PTA, PTI, PTL
      • Parker Tap Adapter for EoE communications
      • User Management in the Parker Automation Controller
      • Using MC_TouchProbe with Compax3 Series Drives
      • Using MC_TouchProbe with P Series Drives
      • Webvis toolbox missing tabs (Codesys calls them tags) - Added alarms but no Alarms Display tool in toolbox.
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?

Print Friendly and PDF

Before downloading and installing PAM 1.4.0.1077 be sure that all desired 1.3.0 projects are saved as “.projectarchive.” Saving projects this way ensures that all 1.3.0 device description files and libraries are included with the project. Failing to import as a “.projectarchive” may cause library and device description conflicts. It is not recommended to open 1.3.0 projects in PAM 1.4.0.1077 from “.project” files.

  1. Within PAM 1.3.0 go to “File” -> “Project Archive” -> “Save/Send Archive…”
  2. A new “Project Archive” menu screen will open. Make sure all boxes (except for Options) are selected when creating a .projectarchive. Options simply saves the current users settings—such as layout and other programming preferences, such as starting screen behavior, what POUs and tabs are currently open during saving, and SmartCoding. General rule of thumb, options is usually left out. Then select “Save…”
  1. You will then be given the option of giving the .projectarchive a name and location to save it in.
  2. Once you have saved all the PAM 1.3.0 projects desired, uninstall PAM 1.3.0.
  3. Restart your computer.
  4. Install PAM 1.4.0.1077.
  5. Restart your computer.
  6. Open PAM 1.4.0.1077
  7. Go to “File” -> “Project Archive” –> “Extract Archive…”
  8. Go to the directory where you have saved your 1.3.0 “.projectarchive” files
  9. A new window will open asking what components you’d like to extract. Extract them all (perhaps except for Options, see note in step 2.)
  10. A few prompts may ask you about overwriting previous files. Read these carefully and answer as needed.
  11. Once opened, a new Project Environment window will open asking if you’d like to upgrade to the latest libraries, compiler, devices, visualization, and SoftMotion versions. Table 1 describes the various versions associated with PAM 1.3.0 versus PAM 1.4.0.1077. Note: By default PAM 1.4.0.1077 does not update to the latest.
  12. Although unnecessary, you can go through the tabs to double-check that the action is set to “Do not update”. When satisfied, select OK to exit the window.

Note, you must either “update all” to PAM 1.4.0.1077 or ensure that you do not update any. Picking and choosing between versions may cause incompatibility issues.

  1. You’re now ready to edit and modify the program the same way you did in PAM 1.3.0.
  2. Note: Without updating you can only download this project to PACs running 1.3.0 firmware even though you are using PAM 1.4.0.1077 to program and edit.
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply