Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Running PMAC motors with the AC30 Drive
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Running PMAC motors with the AC30 Drive
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
  • AC/DC Industrial Drives-
    • AC10+
    • AC30-
      • AC30 Firmware revisions and numbering scheme
      • AC30 Frames K / L / M / N depth dimensions (D) are incorrect in the catalog
      • AC30 MODBUS-TCP EXAMPLE TO INTERACT XPRESS HMI (XTA)
      • AC30 Variations
      • Available I/O
      • How can the AC30 be programmed?
      • How does the control word and status word in the AC30 work?
      • HOW DOES THE INVERSE TIME (OVERLOAD) FUNCTIONALITY PROTECT THE DRIVE (AC30)?
      • How to setup communications on an AC30V with CoDeSys firmware, to a TS8000 with Modbus?
      • How to use the Scope Feature for the AC30 in PAM 1.4
      • Running PMAC motors with the AC30 Drive
      • There is an Extra Library that is added when adding a AC30 Device to a PAM 1.4 project?
      • Updating PDD, using PAM 1.4 to setup an AC30 project, and connecting to an AC30 within PDD.
      • Updating PDQ to the latest version
      • What does the "STK" number mean on my AC30's heatsink?
      • Where to find default configurations on the AC30?
      • Why can't PDQ find my AC30?
      • Why won't my AC30 clone from an SD card?
    • DC590+ Series+
    • AC890 Series+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • AC15/AC20
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
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
Running PMAC Motors with an AC30 Drive

Print Friendly and PDF

The AC30 can run PMAC motors in both Sensorless Vector and Closed Loop Vector modes. Despite many motors being in the motor wizard, you may have to run through this additional troubleshooting document to setup phases, electrical offsets, etc.

The following document will help with setting up an AC30 drive to run PMAC: 3010.PMAC_AC30 FAQ.pdf

This Flow Chart from the manual calls out the steps to program the drive for a PMAC motor: AC30_PMAC_Flowchart.pdf

[QuickLink for the AC30 on Parker.com - Manuals, QuickStarts, Product Support, etc] - The manual found here can provide greater insight to the above documents.

9/20/2018 STV - Created

1NOV19 JD Update

  • PMAC
  • troubleshoot
  • AC30
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply