Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base What are the basic parameters to run an AC Induction motor from just the keypad?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base What are the basic parameters to run an AC Induction motor from just the keypad?
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
  • AC/DC Industrial Drives-
    • AC10-
      • AC10 Heat Dissipation
      • AC10: Is the keypad detachable during operation?
      • AC10: Why am I getting over-voltage trips?
      • AC10: Why is my AC motor running hot?
      • Can I program through the keypad and DSELite on the AC10?
      • How can I configure an AC10 to run at two different speeds without using an analog input?
      • How do I connect an AC10 to a TS8000?
      • How do I clone the AC10 with the 1002-00 module?
      • How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and PDB?
      • How do I implement a Fast Stop circuit on the AC10?
      • How do I know what firmware revision my AC10 is?
      • How do I reset an AC10 back to factory defaults?
      • How do I reset the master password in an AC10?
      • How do I set up an AC10 for torque control?
      • In what type of package is the AC10 available?
      • What are the basic parameters to run an AC Induction motor from just the keypad?
      • What are the basic wiring connections of the AC10?
      • What are the environmental operating conditions for the AC10?
      • What are the minimum and maximum 3-phase input voltage ratings for the AC10?
      • What default configurations are available for the AC10?
      • What is the current overload rating for the AC10 drive?
      • What kind of I/O is available on the AC10?
      • What safety standards does the AC10 meet?
      • What software and communication cable are used for programming an AC10?
      • Why won't my AC10 run my motor?
      • AC10 Modbus-RTU Example to Interact Xpress HMI (XTA)
      • Can an AC10 run a PMAC motor?
      • How does the password protection feature work in the AC10 (via DSE Lite)?
      • How does the password protection feature work in the AC10 (via the keypad)?
      • Updated Control Terminal Torque Specifications for AC10 VFD’s
      • When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.
      • Where do I get the AC10's Modbus RTU / programming connector?
    • AC30+
    • DC590+ Series+
    • AC890 Series+
    • AC15/AC20+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
    • Constant Torque (CT) versus Variable Torque (VT) in VFDs
    • DSE890 and DSELite Ethernet Connection Port Numbers
    • ACxx scope tool problems with Windows 11
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
What are the basic parameters to run an AC Induction motor from just the keypad?

Print Friendly and PDF

To run an AC induction motor on the AC10 in a new application consult the Quickstart guide, on the product page for the AC10 on Parker.com - [Manual, QuickStarts, Product Support, etc].

Below are the minimum parameters that need to be set to run an AC induction motor from just the keypad. Descriptions of these parameters can be found in the manual on the product page, at the link above. If you have already done some programming on the AC10 you can reset the drive to factory defaults by setting F160 = 1.

Motor Data Parameters With Required Values:

  • F801 (Rated Power [kW]) = Motor Nameplate Value
  • F802 (Rated Voltage [V]) = Motor Nameplate Value
  • F803 (Rated Current [A]) = Motor Nameplate Value
  • F804 (Number of Motor Poles) = Motor Nameplate Value
  • F805 (Rated Rotary Speed [RPM]) = Motor Nameplate Value
  • F810 (Motor Rated Frequency [Hz]) = Motor Nameplate Value

Control Parameters With "Keypad Only" Values:

  • F200 (Source of Start Command) = 0
  • F201 (Source of Stop Command) = 0
  • F203 (Main Frequency Source) = 0
  • F207 (Frequency Source Selecting) = 0

Speed Parameters With Starter Values:

  • F106 (Control Mode) = 2
    • 2 is V/Hz Mode
  • F111 (Max Frequency [Hz]) = F810
  • F113 (Target Frequency [Hz]) = [User Defined]
    • The drive ramps to this value when a RUN command is initially given. Set to [F810] for motor nameplate frequency.
  • F118 (Base Frequency [Hz]) = F810

 

10/19/2018 Created STV

12SEP19 JD - Update

  • quickstart
  • AC10
  • frequency
  • basic
  • control
  • keypad
  • run
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply