Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base InteractX Troubleshooting - Can not get License Activation to work on HMI/PC running InteractX version 1.x to 3.4
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base InteractX Troubleshooting - Can not get License Activation to work on HMI/PC running InteractX version 1.x to 3.4
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)+
    • InteractX-
      • InteractX Misc - Cannot find product code for Win9X/NT
      • InteractX Misc - Comm Server Connection to Allen Bradley Logix Processors
      • InteractX Misc - Comparison of valid operators in InteractX versus Interact
      • InteractX Misc - How do I get my InteractX project off of my old unit and onto my new IPX Powerstation?
      • InteractX Misc - How to order InteractX Upgrades
      • InteractX Misc - How to re-register older versions of Interact X (versions 1.x through 3.4)
      • InteractX Misc - How to Start InteractX Runtime Project Automatically?
      • InteractX Misc - Is InteractX Version 1.x, 2.x or 3.x Compatible with Windows 7 or Later?
      • InteractX Misc - InteractX Browser Tool used to display Xpress or PFD screens impacted by Adobe Flash EOL.
      • InteractX Misc - InteractX Software Archive
      • InteractX Misc - Language Multi-Byte Character Support for ASCII Input - Cyrillic, Asian etc...
      • InteractX Misc - Migrating InteractX from legacy HMI and PC systems to Current Hardware and Windows OS Versions
      • InteractX Misc - Uploading and downloading InteractX projects over Ethernet
      • InteractX Misc - Uploading and downloading InteractX projects with a USB drive
      • InteractX Misc - User Configurable Driver User Guide (UCON)
      • InteractX Misc - Version 4.0/4.1 Security Device Questions
      • InteractX Misc - Where does my Powerstation store my InteractX license activation?
      • InteractX Misc - Which HMI runs InteractX?
      • InteractX Software - Complete Modbus/RTU Addressing Example for P Series Indexer Drive
      • InteractX Software - Express Browser Demo
      • InteractX Software - How do I control the Lens States for an Indicator tool in Int X?
      • InteractX Software - How to Shutdown InteractX and Windows
      • InteractX Software - How to Use Existing Recipes as Items within a New or Modified Recipe
      • InteractX Training - Creating and Configuring Event Logs in InteractX
      • InteractX Training - Creating Databases and Tables in InteractX
      • InteractX Training - Database Basics
      • InteractX Training - Getting Started with Quicklogging
      • InteractX Training - Print a Report from InteractX using a VBA form to create your Report layout and VBA logic to populate it.
      • InteractX Training - Recipe Training Module
      • InteractX Training - SQL Database - Basics to use Logging Tools and how to use VBA SQL Script to read data back.
      • InteractX Training - Tag Rules (Tag Sharing) Examples
      • InteractX Training - VBA Login Example
      • InteractX Troubelshooting - ACR9000 CIP Communications stop on all devices when one CIP device goes offline
      • InteractX Troubleshooting - Version 4.1 will not automatically start on my Windows 10 Runtime PC due to requiring elevated privileges
      • InteractX Troubleshooting - Alarm History Viewer not working as expected (InteractX version 4.1)
      • InteractX Troubleshooting - Allen Bradley ControlLogix Driver Compatibility Issues.
      • InteractX Troubleshooting - Can not get License Activation to work on HMI/PC running InteractX version 1.x to 3.4
      • InteractX Troubleshooting - Com Server Error Log
      • InteractX Troubleshooting - COMM Server still using old configuration after download of application with changes to communication settings.
      • InteractX Troubleshooting - ControlLogix Driver unable to upload tags from Device (PLC) unable to read known good tags from processor.
      • InteractX Troubleshooting - CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • InteractX Troubleshooting - Error Initializing VBA when going into run mode or opening the VBA Editor in Development
      • InteractX Troubleshooting - Hardware License Not Found - One Hour Runtime - Remote Desktop
      • InteractX Troubleshooting - InteractX 4.0 HASP key driver Aladdin vs Sentinel (NOTE: IntX4.1 for Windows 10 uses Sentinel Drivers)
      • InteractX Troubleshooting - Invalid Page Fault in the NTOSKERNEL.EXE (old PC/PX models)
      • InteractX Troubleshooting - Loss of Characters on the Pop-up Keyboard, Keypad, etc.
      • InteractX Troubleshooting - Problems with large number accuracy
      • InteractX Troubleshooting - Downloaded InteractX application with Ethernet driver fails to connect even though ping is successful and works otherwise
      • InteractX Troubleshooting - VBA is not working on my new Windows 7/8.1/10 PC (Versions 4.0 / 4.1)
      • InteractX Troubleshooting - Unable to get Data Connection to Xpress tags to work.
      • InteractX Troubleshooting - Why can't I log data with Microsoft Jet (MDB file) in InteractX?
      • InteractX Misc - How to Edit Text Alt+Double-click
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
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
InteractX Troubleshooting - Can not get License Activation to work on HMI/PC running InteractX version 1.x to 3.4

Print Friendly and PDF

The old InteractX versions 1.x - 3.4 had a "soft" License that was stored on the hard drive and could be "lost" under certain conditions.

If the hard drive failed on the PC or HMI hardware older than the HPX series, the license needs regenerated on the new hardware. Later versions of the Parker HMIs had the runtime license embedded in the mother board hardware.

The license could become corrupted since it is just files on the hard drive and a few times over the years, anti-virus and drive compacting utilities have wiped it out. 

Getting relicensed requires your Product Code which is printed on a sticker on the back of the Parker HMIs and would have been on a printed proof of purchase License sheet sent out with stand alone runtime or development software. Running the utility also requires a "hardware code" which the License manager generates.

To use the Product Code to get a new enable code, you need to send it to emn.service@supportparker.com and tell us that you lost your license and we can reset it so it can be used to generate a new License. If it does not get reset, when you try to use it the License manager will tell you no more installs exist for this number. The code is single use and to re-use, we need to unlock it for one more use.

NOTE: Hardware codes are generated dynamically on the HMI or PC on which the license will reside. This code can not be used to license other units and is time sensitive. When licensing a unit, do not generate the hardware code till you are ready to do all of the steps to get and enable the license. The maximum time a code will be good is 24 hours if everything falls just right. It could be much shorter if any other installs are run or changes occur to the hardware which makes the hardware code change.

The Enable Code (Code sent back to your unit from the License activation server) is specific to the unique combination of Hardware Code (dynamically Generated on unit to be licensed) and Product Code (The code you receive printed on the unit product stickers or Paper proof of purchase License document) The hardware code and enable code are both single use and when the enable code is validated, the hardware code changes and the enable code can no longer be used.

InteractX has a built in license manager that can get a new license automatically if the unit is attached to the Internet. If not connected to the Internet the utility has a provision for getting the license off-line via a Web site www.ctcusa.com\registerinteractx which will walk you through the licensing process.

Details for using the license manger are in the following FAQ

Registering old InteractX versions for "soft" license

In the case where you follow all the directions in the How to license FAQ and it looks like the registration worked but when you reboot, it shows 1 hour runtime, you will need to follow the directions in the following PDF before getting the Enable Code reset by apps support and generating a new hardware code.

ReinstallCryptKeyLicenseManager.zip

Be sure to follow all the steps, especially the settings for Windows File Explorer. If any files referenced in the instructions are not deleted, the reinstall of the Cryptkey will not be complete. In some cases the files are actually not there due to Windows issues so as long as the Windows File explorer has the correct settings, it is OK to complete the steps and try to do the license activation.

dm11022018

  • InteractX
  • Product Code
  • Hardware Code
  • Enable Code
  • License