Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Control Access to Panels and Tools using the Password User Levels in Interact
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Control Access to Panels and Tools using the Password User Levels in Interact
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
  • Visualization and Human Machine Interface (HMI)-
    • Interact (Legacy)-
      • Replace/Upgrade Interact panel P11/P1H/P15/P2/P3/P4/P5 etc
      • CTC and i-Motors
      • Configure a TCP/IP Dial-Up Adapter Connection.
      • Interact Misc - Can ASCII register in the PLC be used as an alarm?
      • Configure a TCP/IP connection (IP address)
      • Compact Flash Disk Transfer using Interact MachineShop Toolbar to Upload and Download
      • ERROR - Invalid Panel list or Key Pad Address.
      • Ethernet download to a CTC Panel.
      • How to Restore Motion Panel.
      • Interact Software - Display alarms in a RMD tool within PTM
      • How to run app on my PowerStation on boot-up?
      • Implementing the New CMOT Driver
      • LEDs on the back of the Profibus card
      • MachineLogic - How do I clear Retentive Memory?
      • MachineLogic - No project on the PLC.
      • Security Key Setup not Installed
      • Single layer SST 5136-PFB-104 card with Interact.
      • TCP/IP Ethernet and a Dial-Up Connection
      • TCP/IP open port failure
      • Can I run Interact 6.X in Windows NT/2K/XP?
      • Can I run Interact7 on my Windows 10 or 7 PC?
      • Configure a TCP/IP connection (DHCP)
      • Configure a TCP/IP direct Ethernet connection
      • CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Enable/disable the screen saver
      • Flashback Utilities for the CTC DOS Based PowerStations - If you have Interact ver 7 it installs all the necessary Flashbacks.
      • HMI Battery Replacements
      • How do I connect my P13, PA or PA2 Interact HMI to DataHighway Plus Network?
      • How do I recalibrate my Interact touchscreen? Or change the panel's ethernet address?
      • How do I show hidden and protected files in Windows?
      • How do I transfer my old Interact application to a newer Interact panel?
      • How to connect my device to Interact? Interact Cable Dictionary
      • How to print graphics from Interact run mode.
      • I upgraded my old hardware to a PA2 and have Vertical Stripes on screen and does not load my application.
      • Interact does not recognize the security key.
      • Interact: Error Initializing AMM - Invalid Logging Path
      • Minimum of NT 4.0 SP3 to install Machine Shop
      • Powerstation Shell on older CTC units
      • Replacing old HMIs that run Interact
      • Upgrading from a PA to a PA2
      • What are Interact Runtime modules?
      • Whats the difference between FLH-0512P and FLH-0512?
      • What internal variable can I use to R/W ASCII?
      • Interact Troubleshooting - WinXP- cannot select options on Toolbar
      • Control Access to Panels and Tools using the Password User Levels in Interact
      • Driver for my Allen Bradley Micrologix 1500 PLC?
      • Fonts and Graphics on Tools broken after Interact Upgrade to Ver 7 to run on PA2 hardware. Application runs but FONT Size or images are wrong.
      • GESNP / GESNPX 9030 / 9070 Serial Com configuration for Interact / PowerStation PA/PA2/P13 etc...
      • I need more fonts for my Interact application.
      • INTERACT How to Order
      • Interact screen size too BIG or too small after upgrade. Only see part of screen or screen compressed in top left corner of display.
      • Legacy Product Page - P1 Series
      • Legacy Product Page - P2 Series
      • Legacy Product Page - P3, P4, P5 and P7 Series
      • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
      • Security Key not found or Not programmed to support Module or Driver
      • Which HMI runs Interact?
    • InteractX+
    • Interact Xpress+
    • IXA / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (Discontinued)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • PFD - Parker Factory Display (Discontinued)+
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Control Access to Panels and Tools using the Password User Levels in Interact

Print Friendly and PDF

Applications Settings - Password setup (Level restrictions that are Global in nature)

Use the Level drop-down list box to select the user level associated with the current user name and password.

Interact supports six user levels numbered from 0 to 5. User level 0 is the highest user level, offering the most privileges; user level 5 is the lowest user level, offering the least privileges. You may assign as many users as desired the same user level number. Interact restricts the following AM runtime functions based on the current user level:

· User level 0 - The operator has access to all application, module, and driver functions.

· User level 1 - The operator is restricted to Run Mode functions. The operator may not access Program Mode functions or exit from Interact.

· User level 2, 3 and 4 - In addition to level 1 restrictions, the operator may not select an application.

· User level 5 - In addition to the restrictions for levels 1 through 4, the operator may not view driver screens.

How the Levels Work to restrict access in your application.

The level itself does not inherently limit access to any tools or panels. That is controlled by layering the user levels in order of accessibility when designing the app.  

Level 5 users can only use tools set to user level 5 access. 

Level 4 users can access Level 5 and Level 4 Panels and tools. 

Level 3 users can access Level 5, Level 4 and level 3 Panel's and tools. 

Level 2 users can access Level 5, though Level 2 Panels and tools. 

Level 1 users can access Level 5, though Level 1 Panels and tools. 

Level 0 users can access everything. 

So, the panels and tools OK for everyone to use are set to Level 5 and the startup user is a Level 5. 

Then panels and tools for a technician could be set to level 4  

Panels requiring a supervisor would be set to level 3 

etc... 

Then to access the button or panel with more restriction, there would be a log on required for the user to enter their user name and password. The visibility and access can both be used to ether hide the tool from users not authorized to use it or just the access setting to keep them from using it when not at the correct security level.

Users are defined in the Application Settings for Password Setup.

The Startup User you select sets the default user level for your application when it first boots.

To restrict access to an entire panel and or all of the tools on a panel, you can set required levels in the "Panel List Setup"

You can also restrict individual tool access using the "Accessibility" tab when defining the tool.

This gives the developer a significant amount of flexibility in designing the application and making sure that users have only the access necessary.

dom11122018

  • INTERACT
  • Access Control
  • Accessibility
  • Password
  • User Level
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply