Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Smart Encoder Compatibility
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Smart Encoder Compatibility
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
  • Other-
    • -E Motor Option
    • AC-03 / AC-07 / AC-10 / AC-15 manuals
    • Battery Replacement for 500 or JSI
    • C/CX Suggested Replacements
    • Cage Code
    • Changing the Configuration of the Compumotor Plus
    • Color Code for Stepper Motor External Encoder
    • Compumotor Plus motor internal potentiometers
    • Controller Cable Drawings
    • Custom Products
    • Daedal to Compumotor Cross Reference
    • Daisy chaining AR-C
    • DC Brushed Motor with the Aries & Gemini
    • Drive Input Power
    • Dumping the 3000 memory.
    • EDC TDC XDC VRP PMC
    • Encoder or Resolver?
    • Ferrite absorber
    • Heat Dissipation within Enclosures
    • How do I change the Btorq.dat file?
    • How do I download software from www.parkermotion.com?
    • How do I get support for my Parker SSD / Parvex division products?
    • How Much Power Do I Need?
    • Inertia Ratio
    • Is Parker Compumotor ISO9000 Certified?
    • KH/KS Error 62
    • KH/KS Motors
    • M-Drive/Motor Compatibility and Matching
    • Mating MS Connectors for KH motors
    • Motion Sizer: No motor/gearhead/actuator database error (No TS torque, Divide by 0)
    • My ARC-C or -D does not fit on my motor.
    • Obsolete Products -- 1990 - 1999
    • Obsolete Products -- 2000 and later
    • Offset voltage on the Compumotor Plus
    • Parker MotionSizer: Stationary Rack, Moving Pinion
    • Parker SBC Replacement products
    • PK130M Ordering Part Number Change
    • PK2 Part Number Change(5/9/97)
    • PMC Motion Controllers (PMC20 & PMC10)
    • Printing From Compumotor DOS-based Applications
    • QM Series Motor Information
    • Refurbished Inventory / Educational Discount
    • Setting the deadband on the VAC.
    • Smart Encoder Compatibility
    • Software for the SV
    • Three wire prox sensor color code
    • Torque Margin
    • Transformer Specs
    • Upgrading A/AX Systems
    • VM15 and VM25 Terminal Breakout Modules
    • What is a single and two speed resolver?
    • What is CE, EMC and LVD?
    • What is difference between CD35M and CD60/80M?
    • Windows 2000 locks up when printing
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
Smart Encoder Compatibility

Print Friendly and PDF

The Smart Encoder option (Q) for the MPP/MPJ (order code 3E), SM/SE, BE, NeoMetric/J series motors were only designed to work with the Aries drive. The Smart Encoder uses the Hall output lines as means of communication with the drive to tell it all the pertinent motor settings. This means that the Hall outputs of the Smart Encoder are not used in the traditional fashion and therefore not compatible with any other drives*.

Note: The transfer of motor settings from the Smart Encoder to the Aries drive takes about 3 seconds every time the drive powers up.

*The Compax3 F12 can be made to work by using hall-less startup (wake & wiggle) to ignore the hall sensor feedback. For the Compax3 F12, the feedback cable would need to be changed to the F-2C1.  A custom motor file will need to be created using the Compax3 Motor Manager software. Here's a link to the videos that step you through this. On the last screen of the Motor Manager, change the standard motor file under Commutation: Digital hall sensor  to Automatic commutation with movement.

Note the video shows Commutation angle for a resolver motor but for an encoder it'd be a pull-down selection:

https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/1236/video-how-to-create-custom-rotary-motor-file-for-compax3

This is shown in the 3rd video of that series at this point in the video:

https://youtu.be/zVkKVGBBrQU?t=349

Note: The newer Pseries cannot be used with hall-less commutation with the Smart Encoder feedback without modifying the F-4A1 cable:

https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2226/hall-less-commutation-with-the-p-drive

Motors can be converted to standard incremental encoder via a repair RMA. Contact your ATC distributor for price quote.