Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How to Extract and Install Parameters to the 590+ Drive using DSE Lite
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How to Extract and Install Parameters to the 590+ Drive using DSE Lite
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
  • AC and DC Drives and Inverters-
    • AC10+
    • AC30+
    • AC690+ Series+
    • AC890 Series+
    • DC590+ Series-
      • How do I start troubleshooting a 590+?
      • What are the basic wiring connections required to run a motor, using the factory default drive?
      • How to Extract and Install Parameters to the 590+ Drive using DSE Lite
      • Why won't my motor run?
      • How can I make sure my DC motor does not have a problem with the Field Windings?
      • Why is my DC motor running hot?
      • 590+: Is the keypad detachable during operation?
      • Can I disable the field to run Brushed PMDC (Permanent Magnet DC motor) on a 590+?
      • Can I select between Manual Speed Reference and Line Speed Trim Setting for the same Analog Input?
      • Can you download a DSELite file into the drive when the drive is running?
      • How can I get the DSELite software the 590+ uses?
      • How can I make sure the motor will not start rotating until the speed pot is at 0?
      • How can I manually tune a 590+ drive to my motor?
      • How can I pre-trip "speed feedback" alarm before the drive trips?
      • How can I replace the control boards in 590+ Frame 1 and Frame 2 drives?
      • How can I set up a 590+ to be a field controller?
      • How can I upgrade a 590+ Frame 1 or 2 drive version 5.x or 7.x to version 8.x - Control Board and Configuration
      • How can the 590+ be programmed?
      • How can the drive configuration be reset to factory defaults?
      • How do I clone my 590+ Drive with the keypad?
      • How do I copy the configuration of one drive to another using the keypad?
      • How do I flash my 590+ drive to a newer Minor Revision of Firmware?
      • How do I know what firmware revision my 590+ is?
      • How do I set up a 590+ External Stack?
      • How to I configure the 590+ for Preset Speeds?
      • Is there anything I can check for a SEQ PRE READY alarm?
      • Modbus TCP/IP Addressing for the 590+ drive with the Ethernet Techbox
      • My DC590+ drive is displaying a Missing Pulse Alarm, what should I do?
      • The 590+ is enabled, but the main contactor doesn't close. Why?
      • Upgrading a control door from a 590 to a 590+
      • What accessories can be added to the 590+?
      • What analog and digital I/O is available on the 590+?
      • What are the Communication options for the 590+?
      • What are the communication settings for the 590+ for the P3 Port?
      • What are the differences between the 590 and 590+?
      • What are the minimum and maximum 3phase input ratings for the 590+?
      • What are the reference power supplies available to terminal connections on the 590+?
      • What are the types of Speed Feedback for the 590+?
      • What is the current overload rating for the 590+ drive?
      • What is the maximum operating altitude for the 590+?
      • What is the operating temperature for the 590+?
      • What safety standards does the 590+ meet?
      • What USB-serial adapter should I use?
      • Why does the drive fault to "Over-Voltage" after the drive is enabled?
      • Why does the drive fault to "speed feedback"?
      • Why does the drive fault to 3 phase-fail after the drive is enabled?
      • What I can I check for a CALIBRATION FAIL trip?
      • 590+ - Transferring a Configuration to a Drive with a Different Power Level
      • 598/599+ Stack Controller Replacements
      • DC590+ Encoder Feedback Card Options
      • DRV Contactor Options (955+ part numbers)
      • HOW DO I CONVERT DC590+ UK/JDE PART NUMBERS TO US PART NUMBERS?
      • Speed Regulation with 590+ Drives
      • Troubleshooting a DC brushed motor
      • What are differences between a Regen and Non-Regen 590+?
      • What does "NET FAIL" indicate in DSE Lite when using a LinkNet Techbox module on my 590+ drive?
      • Why is every light on the keypad flashing on my 590+?
    • TS8000, DSI3, & DSI8000+
    • Legacy/Discontinued VFD Products+
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
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
How to Install and Extract Parameters from a 590+ drive

Print Friendly and PDF

***Note that this procedure does not apply for Link or LinkNet 590/590+ Drives***

[QuickLink for more Documentation for the 590+ on Parker.com] - Manual, QuickStarts, etc

If you are unsure of what cable and programming that you need to connect to your 590/590+ drive, the following Knowledge Base post will help: What software and cables will you need to connect to your Parker Drive?

Connecting to the 590+ Drive:

  1. Once the CM351909 programming cable is plugged into both the 590+ and the computer, open up DSE Lite.
  2. You should see a yellow serial port button underneath the “Command” menu. Click on it and select the Com Port that you are connecting through and check that baud rate is set to Auto.
  3. When you select the Com Port that you are using your scratch pad should display a message similar to the one below.
  4. You are now successfully connected to the 590+ drive.
    1. You can now install a template to the drive, extract the parameters from the drive, or go Online with the drive to monitor/toggle parameters.

**Note the version of the the 590P drive, in this example it is a version 8.10 drive meaning that it has version 8.10 firmware.

Extracting Parameters from the 590+ Drive: 

  1. Once you are connected to the 590+ drive you must open a template; the template version is of the same major firmware revision on the drive.
    • In this example our drive has version 8.10 firmware so we will need to open up a Ver8 template. A v7.4 firmware will need to open up a Ver7 template, etc.
  2. Once this template is open you can go to COMMAND > EXTRACT DRIVE PARAMETERS. The following message should appear in the scratch pad in DSE Lite.
  3. When the extract is complete you will see a done appear in the scratch pad. The line should now look similar to this.

How to Install Parameters to the 590+ Drive:

  1. Open the file that you are going to install onto the 590+ drive. Be it a premade template or a saved project
  2. Now you have two options for installing.An “Install” and a “Full Install”. 
    1. An “Install” will install all the parameters in the programming EXCEPT the frame dependent parameters.
    2. A “Full Install” will install all the parameters in the programming INCLUDING the frame dependent+motor data parameters (all purple parameters)
    3. You will usually use the “Install” function unless you are cloning a drive (must be an exact drive replacement). If using the "Install" function do not forget to implement your motor data and run an autotune before running the drive.
  3. Once you have selected the proper function to install the template your scratch pad will populate with a message similar to the one below.
  4. When it is complete you will see a message similar to the one below.

stv 1/8/2019 

9DEC19 JD update

  • DSELite
  • Install Parameters
  • Extract Parameters
  • 590+
  • 590