Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How to Install and Extract Parameters From a 890 or 890PX Drive Using DSE Lite?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How to Install and Extract Parameters From a 890 or 890PX Drive Using DSE Lite?
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
  • AC/DC Industrial Drives-
    • AC10+
    • AC30+
    • DC590+ Series+
    • AC890 Series-
      • What are the basic wiring connections for the AC890?
      • What software and communication cable are used for programming an AC890?
      • How to Install and Extract Parameters From a 890 or 890PX Drive Using DSE Lite?
      • 890 - Interact Xpress with the AC890
      • 890: Why am I getting over-voltage trips?
      • 890PX - Proper ethernet cable - Current Balance, Undervoltage, Missing Phase
      • Can I clone an 890 drive via the Keypad?
      • Can the AC890 be configured as an Active Front End (AFE)?
      • Can the AC890 be used in a load-sharing application?
      • Can the AC890 be used in an electronic lineshaft application?
      • Can the AC890 be used in an encoder following application?
      • Converting .001 file types to .prj file type
      • How can I get the DSE software?
      • How can I get the DSELite software?
      • How can I load different firmwares?
      • How can I recover from a COMMS CODE N error on the AC890
      • How can I troubleshoot Firewire problems?
      • How can the 890 family be configured?
      • How can the AC890 be reset to factory defaults?
      • How can you add an item to the OPERATOR MENU in an AC890?
      • How do I determine an 890 drive TAG NUMBER so it can be used in DSE890?
      • How do I know what firmware revision my AC890 is?
      • How do I make an 890 Phase move?
      • How do I startup & troubleshoot a PMAC motor on the 890?
      • Is the keypad detachable during operation?
      • Is there any additional information on troubleshooting 690+ and AC890 Frame K drives? (copy)
      • My 890 control board locked up when updating the firmware, how can I reset the control board?
      • The AC890 is enabled, and START is true, but the motor runs slow with high torque. Why?
      • The AC890's DC bus voltage is extremely high on power-up. Why?
      • The AC890PX DC bus voltage is extremely high on power up. Why?
      • What are the minimum and maximum 3-phase input voltage ratings on an 890SD, CD, CS and PX?
      • What are the reference power supplies available to terminal connections on the AC890?
      • What can I use to replace an 8902/RR/00/00?
      • What configurable I/O is available on the AC890?
      • What is the current overload rating for the AC890 drive?
      • What is the maximum operating altitude for the AC890?
      • What is the operating temperature for the AC890?
      • What kind of I/O is available on the AC890?
      • What options can be added to the AC890/890PX?
      • What safety standards does the 890 meet?
      • What slots I can put options in, and how do I install them?
      • What types of speed feedback are supported for the AC890?
      • Where do I find default configurations?
      • Why am I getting an Incompatible Power Board message?
      • Why can't I connect to my AC890 drive with the USB cable
      • Why is my AC motor running hot?
      • Why is the LED on the control board flashing 50% red and 50% green?
      • Why won't DIN3 stop my 890 drive with a default configuration in remote mode?
      • Why won't my AC890 inverter run my motor?
      • AH469479U001 card - Use 8903/??/00/00 when ordering replacements
      • AH469910U001 - Use 8904/A/US/03/00 or 8904/A/US/03/83 to order replacements
      • How do I convert AC890 Europe part numbers to US part numbers?
      • HOW DOES THE INVERSE TIME (OVERLOAD) FUNCTIONALITY PROTECT THE DRIVE (890)?
      • Runtime alert when connecting to or downloading a project to an 890 drive - DSEv3.10
    • AC15/AC20+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
    • Constant Torque (CT) versus Variable Torque (VT) in VFDs
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
How to Install and Extract Parameters From a 890 or 890PX Drive Using DSE Lite?

Print Friendly and PDF

***Note that this procedure does not apply for Link, LinkNet, or Firewire 890 Drives***

[QuickLink for the 890 on Parker.com] - Manual, QuickStarts, Product Support, etc

[QuickLink for the 890PX on Parker.com] - Manual, QuickStarts, Product Support, etc

If you are unsure of what cable and programming that you need to connect to your 890 drive, the following FAQ post will help: What software and cables will you need to connect to your Parker Drive?

Connecting to the AC890 Drive:

  1. In order to connect to the AC890 drive you will have to install the USB drive for the 890 Drive. Installation instructions can be found under the "HELP" menu, by clicking on the Installing USB drives tab. Follow this procedure before continuing or you will be unable to connect to the drive.
  2. Once the CM471050 programming cable is plugged into both the AC890 (via the miniUSB port on the control panel of the drive) and the computer, open up DSE Lite.
  3. You should see a yellow serial port button underneath the “Command” menu. Click on it and select the Com Port that you are connecting through and check that baud rate is set to Auto.
  4.  When you select the Com Port that you are using your scratch pad should display a message similar to the one below.
  5. You are now successfully connected to the AC890 drive. You can now install a template to the drive, extract the parameters from the drive, or go Online with the drive to monitor/toggle parameters.

**Note the version of the AC890 drive, in this example below it is a version 3.15 drive meaning that it has version 3.15 firmware.

 

Extracting Parameters from the AC890 Drive:

  1. Once you are connected to the AC890 drive you need to go to FILE > EXTRACT to extract the parameters from the drive.
    • This also extract drive-dependent parameters, unlike other products. 
  2.  The following message should appear in the scratch pad in DSE Lite when the programming is being extracted from the AC890.
  3. When the extract is complete you will see a done appear in the scratch pad. The line should now look similar to this.
    •  

How to Install Parameters to the AC890 Drive:

  1. Open the template that you are going to install onto the AC890 drive. Now you have two options for installing, an “Install” and a “Full Install”.
    1. An “Install” will install all the parameters in the programming EXCEPT the frame dependent parameters.
    2. A “Full Install” will install all the parameters in the programming INCLUDING the frame dependent parameters.
    3. You will usually use the “Install” function unless you are cloning a drive (must be an exact drive replacement). If using the "Install" function do not forget to implement your motor data and run an autotune before running the drive.
  2. Once you have selected the proper function to install the template your scratch pad will populate with a message similar to the one below.
  3. When it is complete you will see a message similar to the one below.
    1.  

STV 1/10/2019

9DEC19 JD update

  • DSELite
  • dse890
  • Install
  • ac890
  • DSE
  • DSE Lite
  • Extract
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply