Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base eCL Homing notes with PAC via EtherCAT
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base eCL Homing notes with PAC via EtherCAT
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
  • Motion and Machine Controllers-
    • ACR Controllers+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)-
      • 3rd Party Samples+
      • Embedded Xpress+
      • Errors+
      • Hardware+
      • PAM IDE+
      • Programming Tips+
      • Web Visualization+
      • Quick Start and Online Training Videos
      • Adding New Devices
      • Auto Addressing enabled by default
      • Cam and Gear Program Sample & Video
      • Common PACIO Troubleshooting Tips
      • Compax3 Linear servo motor settings with PAC
      • Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
      • Reading G Code from a file to develop a CNC machine
      • Error: Red triangle on EtherCAT axes/devices when ModBus or ProfiNet connects
      • FTP support
      • How can I send ASCII strings to or from the PAC?
      • How do I configure and gear to the PACIO-454-01 Module?
      • How do I upgrade a Parker Automation Manager (PAM) project from 1.3.0 to 1.4.0?
      • How do I use variables in G code?
      • How to Add ModbusTCP to PAC project (PAC as ModbusTCP slave)
      • How to Set and Get Time / Date / Time Zone Pre-1.4
      • How to Update Devices and their Descriptor files
      • How to Update PAC project without Parker Automation Manager software?
      • How to Update a PAC Firmware? Flashback instructions
      • How to Upload a Program?
      • How to Use the InteractX OPC Quick Client with the PAC
      • How to set up EtherNet/IP Communications with an Allen Bradley PLC
      • How to set Scaling for Parker Mechanics
      • How to use the Outputs on the Compax3-I31 or P series (EtherCAT)
      • IO settings for EtherCAT_Master: How to see IO update while in Stop
      • Log Data to a File
      • Minimum Internet Explorer version for Xpress and Visualization options
      • PAC CNC & Multi-Axis Capabilities, Samples & Video demos
      • PAC CNC visualization
      • PAC System Time Access and Edits
      • PAC Web Visualization with Internet Explorer: missing browser feature HTML5-Canvas Webvisu
      • PAC with .Net or LabView or InteractX: Using OPC DA Server
      • PAC with Modbus: What addresses for tags?
      • Reading Torque from Pseries drive
      • Remanent Variables: Retain vs Persistent Retain
      • Retentive Memory details
      • SDO Read / Write PAC to/from Compax3 I31
      • SMC_ERROR.SMC_FB_WASNT_CALLED_DURING_MOTION
      • Sample Continuous Function Chart CFC Program: time based counter
      • Sample Continuous Function Chart CFC Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Time based counter
      • Sample SFC Program: time based counter
      • Sample Stuctured Text ST Program: Time Based Counter
      • Sample Structured Text ST Program: Basic Motion (Power, Home, Cycle)
      • Single Axis Sample Program with Visualization
      • Two Axis Sample Program with Visualization
      • Using the PAC as a Modbus TCP Master Device
      • Using the PAC as a Modbus TCP Slave Device
      • VIDEO: Run an AC30V an AC Induction motor via EtherCAT with a PAC
      • VIDEO: PAC with Compax3 EtherCAT part 1: EtherCAT connections & Device Selection
      • VIDEO: PAC with Compax3 EtherCAT part 2: Complete Configuration
      • VIDEO: PAC with Compax3 EtherCAT part 3: Setting EtherCAT Master and DS402 scaling
      • VIDEO: PAC with Compax3 EtherCAT part 4: Download & Test in C3 ServoManager
      • Video: Parker's PAC, the Automation Controller Based on IEC61131-3
      • What's the 16# in the axis scaling default of 16#10000?
      • Working with recipes in the PAC
      • Does the PAC have a first scan flag?
      • Error when switching Active Application
      • Using tappets during cam motion
      • WebVisualization not working in PAC terminal (PTA)
      • Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
      • Does PAC act as a OPC-UA server or client, or both?
      • How do I upgrade the PAC from OPC-DA to OPC-UA?
      • How do I use OPC-UA with the PAC?
      • PACIO-441-01 analog current input module
      • Sample code for PACIO-442-02 and PACIO-441-02 analog modules
      • What ports get used with PAC Ethernet connections?
      • C0032: Cannot convert type 'Unknown type: 'ADR(Device.Application.PLC_PRG.x)' to type 'POINTER TO BOOL'
      • CSV Reader Library for the PAC
      • Do I have to upgrade my PAC 1.3.0 Firmware to work with a PAM 1.4.0 project?
      • eCL Homing notes with PAC via EtherCAT
      • EtherCAT communication between the PAC and AC30 drive
      • How to add images to a visualization in WebVis
      • How to reset the EtherCAT bus
      • Parker Tap Adapter for EoE communications
      • User Management in the Parker Automation Controller
      • Using MC_TouchProbe with Compax3 Series Drives
      • Using MC_TouchProbe with P Series Drives
      • Webvis toolbox missing tabs (Codesys calls them tags) - Added alarms but no Alarms Display tool in toolbox.
    • 6K (Discontinued)+
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
      • Electromechanical – Mobile Forums
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
eCL Homing notes with PAC via EtherCAT

Print Friendly and PDF

Use SMC3_ETC_WriteParameter_CoE to do a SDO (acyclic 'one-shot' data write) to the eCL to set the Homing Speed and Homing Mode before doing an MC_Home.

Index and subindex are listed in eCL user manual.

eCL_PAC.txt
PROGRAM PLC_PRG
VAR

	YPower: mc_power;
	bTurnOnY: BOOL;
	
	Ymove: SM3_Basic.MC_MoveRelative;
	bMoveY: BOOL;
	Yhome: SM3_Basic.MC_Home;
	bHomeY: BOOL;
	
	YSetHomingMode:SM3_Drive_ETC.SMC3_ETC_WriteParameter_CoE;
    bYSetHomingMode:BOOL;	
	
	YSetHomingSpeed:SM3_Drive_ETC.SMC3_ETC_WriteParameter_CoE;
    bYSetHomingSpeed:BOOL;	

END_VAR



YPower(
	Axis:= Y, 
	Enable:=	TRUE, 
	bRegulatorOn:= bTurnOnY, 
	bDriveStart:= bTurnOnY, 
	Status=> , 
	bRegulatorRealState=> , 
	bDriveStartRealState=> , 
	Busy=> , 
	Error=> , 
	ErrorID=> );
	
	Ymove(
	Axis:= Y, 
	Execute:=bMoveY , 
	Distance:= 1, 
	Velocity:= 1, 
	Acceleration:=10 , 
	Deceleration:=10 , 
	Jerk:= , 
	Done=> , 
	Busy=> , 
	CommandAborted=> , 
	Error=> , 
	ErrorID=> );

YSetHomingMode(
	xExecute:=bYSetHomingMode, 
	xAbort:= , 
	uiIndex:=16#6098 , 
	usiSubIndex:= 0, 
	usiDataLength:=1 , 
	dwValue:= 1, 
	Axis:= Y, 
	xDone=> , 
	xBusy=> , 
	xError=> , 
	dwErrorCode=> , 
	eError=> );
	
YSetHomingSpeed(
	xExecute:=bYSetHomingSpeed, 
	xAbort:= , 
	uiIndex:=16#6099 , 
	usiSubIndex:= 1, 
	usiDataLength:=4 , 
	dwValue:= 10000, 
	Axis:= Y, 
	xDone=> , 
	xBusy=> , 
	xError=> , 
	dwErrorCode=> , 
	eError=> );
	
Yhome(
	Axis:=Y , 
	Execute:= bHomeY, 
	Position:= 0, 
	Done=> , 
	Busy=> , 
	CommandAborted=> , 
	Error=> , 
	ErrorID=> );

ECLD-4DC-PC  EtherCAT Stepper drive wiring for Limit Sensors (Limit+, Limit-, Origin; and Inputs & Outputs)

aka End of Travel and Home inputs

NPN sensors required with wiring shown.