Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Sequence Select Inputs (OEM750X)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Sequence Select Inputs (OEM750X)
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
  • Legacy (Discontinued)-
    • 4000+
    • Compax and SV+
    • 6000+
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX+
    • iBE+
    • 630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)
    • L20+
    • MP-FLX and FLX+
    • MPA Servo Drives+
    • Motion Architect+
    • PC21+
    • RP240+
    • S/SX Drives+
    • OEM Products-
      • Battery OEM:010,070,650X-M2,670X/675X,750X-M2,770X
      • CE marking for the OEM 1000
      • Changing a OEM350X/650X/750X to an OEM350/650/750
      • Changing an OEM670X/675X to an OEM670T/675T
      • Changing the Direction of Steppers
      • Configuring OEM servo drives for BE motors
      • Current loop compensation resistor
      • DC Brushed Motor with the OEM670 & OEM 675
      • DC Brushed Motor with the OEM770
      • Do not Wire OEM300 in Series or Parallel
      • Enable in for the OEM750/750X
      • How do I find an OEM device address?
      • I cannot disable my OEM750.
      • Nested Loops in OEM and PDX
      • OEM Fault Input
      • OEM Products: Connector Part Numbers
      • OEM Resistor Kit
      • OEM Servo Motor Specifications
      • OEM350/OEM650 Product Change Notification
      • OEM670 Changing Directions
      • OEM67n peak current, resistor selection
      • OEM750 drive shutdown / remote input?
      • OEM750/OEM750X Connector Part Number
      • OEM750X Minimum Voltage Requirements
      • OEM750X on Power Up
      • OEM770 replaces the OEM670/675
      • OEM770 Resistor Kit
      • OEMZL4 replaced by ZETA4, OEMZL6 still available
      • Sequence Select Inputs (OEM750X)
      • TQ10 and OEM67n Hall Sensor Compatibility
      • TR Command in Basic X Products
      • Uploading in an X-language product.
      • What is the step pulse output width for OEM010?
      • X Language Products - Communication via RS232
    • SFD Servo Drives and SF Servo Motors+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
    • Legacy Product Page - Luge LM Series
    • Parvex Motion Explorer and Easy Rider Software
    • Running the SMA with a DC Brushed Motor
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
Sequence Select Inputs (OEM750X)

Print Friendly and PDF
The sequence-select inputs for the OEM750X require the -M2 option (expanded memory) to be installed.

The following commands also apply to the OEM010 / 070.

The XP command activates Sequence Run On Powerup. If XP is set to something between 1-7, that sequence# will be automatically executed on powerup. If XP is 8, the OEM will read whatever sequence is selected with the Sequence Select inputs (SEQ #3 = Most Significant Bit). XP9 is the same as XP8, except that with XP9, once it is finished with the program, it will read the sequence select inputs again and then execute that sequence.

XQ is a setting that affects operation during XP9 mode. The difference between XQ0 and XQ1 is that XQ1 requires all inputs to drop low (that is, it must read a binary 0) before the next sequence can be selected. If this has not happened by the time the first sequence has finished executing, the OEM will not run the currently selected sequence; it will wait until all inputs read 0; then, as soon as it sees a nonzero value, it will start that sequence.