Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How can I flash the LinkNet Techbox firmware?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How can I flash the LinkNet Techbox firmware?
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
  • AC and DC Drives and Inverters-
    • AC10+
    • AC30+
    • AC690+ Series+
    • AC890 Series+
    • DC590+ Series+
    • TS8000, DSI3, & DSI8000+
    • Legacy/Discontinued VFD Products+
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
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
How can I flash the LinkNet Techbox firmware?

Print Friendly and PDF

1 - Connect to the Techbox (with either an Ethernet cable or the USB cable)

2 - Start DSE-Lite

3 - Choose the correct COM

4 - Check to see you are connected (It will say in the scratchpad to what the software is connected and what firmware is installed in the unit)

5 - Choose COMMAND - INSTALL FIRMWARE

6 - Click OK

 7 - Choose Firmware version

8 - DO NOT INTERRUPT

9 - Check version (verify in the scratchpad that the new firmware is installed in the unit)