Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How can I troubleshoot Firewire problems?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How can I troubleshoot Firewire problems?
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
  • +Motion and Machine Controllers
  • +General Technology Information
  • +Virtual Engineer
  • +Visualization and Human Machine Interface (HMI)
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • -AC and DC Drives and Inverters
    • +AC10
    • +AC30
    • +AC690+ Series
    • -AC890 Series
      • What are the basic wiring connections for the AC890?
      • What software and communication cable are used for programming an AC890?
      • How to Install and Extract Parameters From a 890 or 890PX Drive Using DSE Lite?
      • 890 - Interact Xpress with the AC890
      • 890: Why am I getting over-voltage trips?
      • 890PX - Proper ethernet cable - Current Balance, Undervoltage, Missing Phase
      • Can I clone an 890 drive via the Keypad?
      • Can the AC890 be configured as an Active Front End (AFE)?
      • Can the AC890 be used in a load-sharing application?
      • Can the AC890 be used in an electronic lineshaft application?
      • Can the AC890 be used in an encoder following application?
      • Converting .001 file types to .prj file type
      • How can I get the DSE software?
      • How can I get the DSELite software?
      • How can I load different firmwares?
      • How can I recover from a COMMS CODE N error on the AC890
      • How can I troubleshoot Firewire problems?
      • How can the 890 family be configured?
      • How can the AC890 be reset to factory defaults?
      • How can you add an item to the OPERATOR MENU in an AC890?
      • How do I determine an 890 drive TAG NUMBER so it can be used in DSE890?
      • How do I know what firmware revision my AC890 is?
      • How do I make an 890 Phase move?
      • How do I startup & troubleshoot a PMAC motor on the 890?
      • Is the keypad detachable during operation?
      • Is there any additional information on troubleshooting 690+ and AC890 Frame K drives? (copy)
      • My 890 control board locked up when updating the firmware, how can I reset the control board?
      • The AC890 is enabled, and START is true, but the motor runs slow with high torque. Why?
      • The AC890's DC bus voltage is extremely high on power-up. Why?
      • The AC890PX DC bus voltage is extremely high on power up. Why?
      • What are the minimum and maximum 3-phase input voltage ratings on an 890SD, CD, CS and PX?
      • What are the reference power supplies available to terminal connections on the AC890?
      • What can I use to replace an 8902/RR/00/00?
      • What configurable I/O is available on the AC890?
      • What is the current overload rating for the AC890 drive?
      • What is the maximum operating altitude for the AC890?
      • What is the operating temperature for the AC890?
      • What kind of I/O is available on the AC890?
      • What options can be added to the AC890/890PX?
      • What safety standards does the 890 meet?
      • What slots I can put options in, and how do I install them?
      • What types of speed feedback are supported for the AC890?
      • Where do I find default configurations?
      • Why am I getting an Incompatible Power Board message?
      • Why can't I connect to my AC890 drive with the USB cable
      • Why is my AC motor running hot?
      • Why is the LED on the control board flashing 50% red and 50% green?
      • Why won't DIN3 stop my 890 drive with a default configuration in remote mode?
      • Why won't my AC890 inverter run my motor?
      • AH469479U001 card - Use 8903/??/00/00 when ordering replacements
      • AH469910U001 - Use 8904/A/US/03/00 or 8904/A/US/03/83 to order replacements
      • How do I convert AC890 Europe part numbers to US part numbers?
      • HOW DOES THE INVERSE TIME (OVERLOAD) FUNCTIONALITY PROTECT THE DRIVE (890)?
      • Runtime alert when connecting to or downloading a project to an 890 drive - DSEv3.10
    • +DC590+ Series
    • +TS8000, DSI3, & DSI8000
    • +Legacy/Discontinued VFD Products
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
  • What replaces the Gemini GV6K servo drive controller?

You are currently reviewing an older revision of this page.

  • History View current version

How can I troubleshoot Firewire problems?

If you're experiencing noise in a Firewire system or it seems to drop-out intermittently the following troubleshooting points need to be done to pinpoint what the issue may be. This is a lot to absorb, but there is no easy answer without monitoring the drives.

In a good operating system, once the Firewire powers up and gets done handshaking with all of the modules, the parameters BUSS RESETS, MY BUSS RESETS and the BAD MESSAGE should not be increasing on the FIREWIRE function block. There will be numbers for these parameters, but once they get done handshaking they should stabilize and not increase. If there are a lot of Buss Resets and My Buss Resets on all the drives, that is not good and indicates an issue somewhere. There should be no more than a couple hundred on each parameter at most.

  1. First make sure that the FireWire cards are powered correctly.
    • The IEEE1394 bus requires a separate, floating 24 Vdc (12-24 Vdc) supply connected to Connector X42
    • NOT connected to the same 24Vdc supply that is connected to X13
  2. To see where the problem may be coming from monitor the BUSS RESETS, MY BUSS RESETS and the BAD MESSAGE parameter on the FIREWIRE block.
  3. Monitor these at each drive while the drive is powered up, but not in the RUN mode. When the IGBT's are not firing and generating noise.
    • If the MY BUSS RESETS is increasing, there is noise on the Firewire from some outside source.
    • If the BUSS RESETS & BAD MESSAGE are increasing it could be a bad Firewire card or Firewire cable.
    • If the parameter numbers are not increasing, it would appear that the hardware is good
  4. Now RUN the drive and the motor. When the IGBT's are firing and power will be going to the motor and the motor leads.
    • Monitor BUSS RESETS & MY BUSS RESETS.  Are they increasing? If so noise from the IGBT's are getting into the Firewire.
      1. Maybe from the motor leads not being wired or grounded properly?
      2. Is the motor cable shielded? On both ends? Is it loose?
  5. RUN one (1) drive at a time and repeat step four to see if the noise or problematic drive can be isolated.

If the LED on the Firewire card is a flashing Amber LED, or if the color is not in the list, it usually means the card is off in the weeds.

  • A flashing amber LED MAY mean that the Buss is continually resetting

Important questions to ask:

How old is the system?

When was it started up?

Has it ever worked correctly?

When did the Firewire issues start occurring?

What changes were made recently?

LS MAR19

Updated/Formatted JD 14MAY19