Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller-
      • IPA Accessories - IPA as Ethernet/IP Scanner for Ethernet/IP I/O Adapter Devices (Video)
      • IPA Cables - P Series Motors to IPA
      • IPA Hardware - Connector Part Numbers
      • IPA Hardware - DC Power
      • IPA Hardware - Does the IPA Have Battery Backed Memory or Flash?
      • IPA Hardware - MX80L Limit/Home Wiring
      • IPA Hardware - Short Circuit Current Rating (SCCR)
      • IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
      • IPA Hardware - What is the minimum regen (braking) resistor value allowed?
      • IPA Misc - Letter of Volatility
      • IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
      • IPA Misc - Absolute Encoder Compatibility (EnDat)
      • IPA Misc - Aries Controller Replacement
      • IPA Misc - How to Calculate Regeneration
      • IPA Misc - How to Change the IP Address
      • IPA Misc - IPA with Allen-Bradley Ethernet/IP with ETH Actuator (Video)
      • IPA Software - Add On Instructions Tutorial for Allen-Bradley Logix PLCs (Training Video)
      • IPA Software - Add-On Instructions
      • IPA Software - Analog Input Parameters, Filtering, Example Joystick Program (Video)
      • IPA Software - Assigning Limit and Home Inputs (HLBIT)
      • IPA Software - Basic Tuning using ACR-View
      • IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
      • IPA Software - Communicating via ASCII over Ethernet TCP/IP
      • IPA Software - Configuration Parameter for the Feedback Type
      • IPA Software - Ethernet/IP with Allen-Bradley or Omron PLCs
      • IPA Software - Example - Ballscrew Compensation / Slope Correction
      • IPA Software - Example - Cable Winding Application
      • IPA Software - Example - Error Recovery Program
      • IPA Software - Example - Excel Spreadsheet to Upload/Download Arrays
      • IPA Software - Example - How to Home to a Hardstop
      • IPA Software - Example - Interact Xpress HMI
      • IPA Software - Example - Torque Limited Move for Clamping (with Video)
      • IPA Software - How does motion work in the ACR products (ARC7xxx, ACR9xxx, IPA, Aries-CE)
      • IPA Software - How to Change the Home Start Direction and Other Home Settings
      • IPA Software - How to Save Servo Gains
      • IPA Software - INTCAP (Position Capture)
      • IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
      • IPA Software - Torque Enable Inputs Functionality
      • IPA Software - User Variables and Bits (Which are retained?)
      • IPA Troubleshooting - Endat Absolute Encoders with IPA-Feedback Errors
      • IPA Troubleshooting - ETT Actuator Noise
      • IPA Troubleshooting - PC communications (Ethernet)
      • IPA Troubleshooting - Watchdog Timeout Event Triggered or Reconnect Event Triggered Error (ACR-View)
      • IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)

Print Friendly and PDF

[Related FAQ: Torque Enable Inputs]

The IPA comes with a two-channel redundant Torque Enable circuit accessible through the X7 connector on the top of the drive.  The drive ships with factory-installed jumpers to bypass this circuit as a convenience to customers who want to do initial bench testing or do not need this feature.  To make use of the Torque Enable circuit, the jumpers will need to be removed and the two Torque Enable channels will need to be energized by an external 24 VDC power supply.

Signal Pin Description
CUST_24V 1 Control keep alive power
TRQ_EN1 2 Torque enable input 1
TRQ_EN2 3 Torque enable input 2
TRQ_EN_24V 4 Bypass power for TE (limited to 30mA)
ANALOG_IN0 5 Differential analog input 0 +/-10V
ANALOG_IN1 6 Differential analog input 1 +/-10V
CUST_COM 7 Common for control keep alive power
/TRQ_EN1 8 Torque enable input 1
/TRQ_EN2 9 Torque enable input 2
TRQ_EN_COM 10 Common for TRQ_EN_24V
/ANALOG_IN0 11 Differential analog input 0 +/-10V
/ANALOG_IN1 12 Differential analog input 1 +/-10V

NOTE: TRQ_EN_24V (the IPA's Torque Enable bypass power supply) is limited to less than 30mA of current by hardware. It is meant only to bypass the Torque Enable functionality in applications that do not require its use. It is not meant to power external circuitry.  Do not use pins 4 and 10 with anything other than the factory-supplied jumpers.  [Link: Page 41 of the IPA Hardware Installation Guide]

An example wiring diagram is given below.  This diagram shows the 24 VDC supply circuit being interrupted by a contact.  If the circuit opens, the motor will immediately lose torque.

NOTE: The diagram below is an example.  While it is electrically valid, different industries and regions have varying safety requirements.  Refer to applicable safety standards to determine what is appropriate for your application.  [Link: Page 6 of IPA Hardware Installation Guide]

It is important to note that opening the Torque Enable circuit WILL NOT bring the motor to a controlled stop.  If the motor is moving when the Torque Enable circuit is opened, it will continue to move until it is stopped by an external force.  This is a particularly important consideration for vertical axes as well as axes that move at high speed.

16APR2019 DCLIFFE

  • circuit
  • diagram
  • IPA
  • wiring
  • X7
  • enable
  • torque
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply