Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Analog control of a Vix stepper
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Analog control of a Vix stepper
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)-
      • Analog control of a Vix stepper
      • Can an Intelligent ViX-In be Programmed as a Drive
      • Configuring the ViX-drive
      • DC Brushed Motor with a ViX
      • Does the Vix have software limits?
      • Downloading Programs
      • Easi-V with Windows 7 or Windows 10
      • Homing move not complete
      • How Do I Check encoder position?
      • How to program an intelligent ViX Stepper as a Step & Direction
      • LOADENC and SCALE Commands
      • Running a Rotary Motor with a ViX-xH
      • Sample Program - Move Continuously, Stop on Inputs
      • VIX - RS232 connections
      • VIX Servo: How to Home to a Hard Stop
      • VIX Update Rates
      • ViX User Variables
      • ViX CANopen / RS-485 option
      • ViX Easi-V Error Message: Invalid data read for limits mode
      • ViX Encoder Resolution / Input Frequency
      • ViX Motor files for non-preferred BE windings
      • ViX Tuning
      • ViX servo drive Z channel encoder output
      • ViX-RJ45 RS-232 Daisy-Chain Cables
      • ViX: Connector Part Numbers
      • ViX: ViX Update Rates
      • Vix- Option 1 (MPM) Encoder Hardware Setup
      • Vix-IE with Brushed motor and Encoder
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Analog control of a Vix stepper

Print Friendly and PDF
All of Parker's stepper drive/controllers can be easily programmed to follow an analog velocity command. The Vix 250/500 IM, however, has this capability built-in. After running the Guided Drive Setup, you only need to issue four commands to get it into Velocity Following mode (also known as Mode Bidirectional).

Assuming address #1,

1MB ;Puts the Vix into Bidirectional mode
1V10 ;This scales the maximum speed to 10rps
1ON ;Enables the Vix
1G ;Starts following the analog input

You may want to issue a 1SV to save this configuration. A reset is not necessary to switch into Mode Bidirectional.

The analog input should be wired into pins 1 & 2 of connector X4. The analog input's voltage range is -10V/+10V, allowing the motor to spin both directions. You can read and write to the parameters AB (Analog Deadband) and AO (Analog Offset) to tweak the Vix's operation. You can also read the analog input voltage with 1R(AI). Units are raw counts (-2047 to +2047).
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply