Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How do I startup & troubleshoot a PMAC motor on the 890?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How do I startup & troubleshoot a PMAC motor on the 890?
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
  • AC/DC Industrial Drives-
    • AC10+
    • AC30+
    • DC590+ Series+
    • AC890 Series-
      • AH469479U001 card - Use 8903/??/00/00 when ordering replacements
      • AH469910U001 - Use 8904/A/US/03/00 or 8904/A/US/03/83 to order replacements
      • What are the basic wiring connections for the AC890?
      • What software and communication cable are used for programming an AC890?
      • How to Install and Extract Parameters From a 890 or 890PX Drive Using DSE Lite?
      • 890 - Interact Xpress with the AC890
      • 890: Why am I getting over-voltage trips?
      • 890PX - Proper ethernet cable - Current Balance, Undervoltage, Missing Phase
      • Can I clone an 890 drive via the Keypad?
      • Can the AC890 be configured as an Active Front End (AFE)?
      • Can the AC890 be used in a load-sharing application?
      • Can the AC890 be used in an electronic lineshaft application?
      • Can the AC890 be used in an encoder following application?
      • Converting .001 file types to .prj file type
      • How can I get the DSE software?
      • How can I get the DSELite software?
      • How can I load different firmwares?
      • How can I recover from a COMMS CODE N error on the AC890
      • How can I troubleshoot Firewire problems?
      • How can the 890 family be configured?
      • How can the AC890 be reset to factory defaults?
      • How can you add an item to the OPERATOR MENU in an AC890?
      • How do I determine an 890 drive TAG NUMBER so it can be used in DSE890?
      • How do I know what firmware revision my AC890 is?
      • How do I make an 890 Phase move?
      • How do I startup & troubleshoot a PMAC motor on the 890?
      • Is the keypad detachable during operation?
      • Is there any additional information on troubleshooting 690+ and AC890 Frame K drives? (copy)
      • LA471585 I/O Break-Out Module (Discontinued)
      • My 890 control board locked up when updating the firmware, how can I reset the control board?
      • The AC890 is enabled, and START is true, but the motor runs slow with high torque. Why?
      • The AC890's DC bus voltage is extremely high on power-up. Why?
      • The AC890PX DC bus voltage is extremely high on power up. Why?
      • What are the minimum and maximum 3-phase input voltage ratings on an 890SD, CD, CS and PX?
      • What are the reference power supplies available to terminal connections on the AC890?
      • What can I use to replace an 8902/RR/00/00?
      • What configurable I/O is available on the AC890?
      • What is the current overload rating for the AC890 drive?
      • What is the maximum operating altitude for the AC890?
      • What is the operating temperature for the AC890?
      • What kind of I/O is available on the AC890?
      • What options can be added to the AC890/890PX?
      • What safety standards does the 890 meet?
      • What slots I can put options in, and how do I install them?
      • What types of speed feedback are supported for the AC890?
      • Where do I find default configurations?
      • Why am I getting an Incompatible Power Board message?
      • Why can't I connect to my AC890 drive with the USB cable
      • Why is my AC motor running hot?
      • Why is the LED on the control board flashing 50% red and 50% green?
      • Why won't DIN3 stop my 890 drive with a default configuration in remote mode?
      • Why won't my AC890 inverter run my motor?
      • How do I convert AC890 Europe part numbers to US part numbers?
      • HOW DOES THE INVERSE TIME (OVERLOAD) FUNCTIONALITY PROTECT THE DRIVE (890)?
      • Runtime alert when connecting to or downloading a project to an 890 drive - DSEv3.10
    • AC15/AC20+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
    • Constant Torque (CT) versus Variable Torque (VT) in VFDs
    • DSE890 and DSELite Ethernet Connection Port Numbers
    • ACxx scope tool problems with Windows 11
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
How do I startup & troubleshoot a PMAC motor on the 890?

Print Friendly and PDF

The 890 series only supports closed loop PMAC control. Sensorless PMAC control is not supported on the 890.

For sensorless PMAC control (or PMAC control on a VFD in general) the AC30 should be considered first. In North America, we initially recommend using products from our traditional servo offering for PMAC motion control; including camming & positioning applications. Your local Parker ATC can provide support for creating these applications. 


The 890 drive with firmware v3.x may be paired with a permanent magnet AC motor (PMAC). European PMAC motors (such as Parker's NX motor line) were often used with the 890. Large PMAC motors such as Parker’s MGV high speed motors, GVM Global Vehicle Motors, and TMW torque motors were also used for 890 PMAC applications.

  • Part 1: Create a PMAC Configuration on an 890:
    •  How to build an 890 configuration for a PMAC motor - Issue B
      • Walks through the motor wizard configurator
        • Selecting a pre-configured Parker motor, or necessary information to implement your own
  • Part 2: Commutating a PMAC for startup, or troubleshooting a PMAC electrical position offset 
    • How to troubleshoot the start-up of a PMAC motor 
      • Pulled from the manual, this procedure must be done to commutate a PMAC motor (the electrical position offset)
        • The commutation procedure uses the 6901 keypad as the small keypad does not have access to these options.
          • With 8 yellow buttons, 1 green RUN button, and 1 red STOP button.
          • The PROG button on the 6901 Keypad is useful for switching back and forth between your location in the menus and running the motor in local mode
        • Walks through tests involving:
          • Inverting the feedback signal with one parameter
          • Rotation direction verification
          • Adjusting the electrical position offset
        • IMPORTANT NOTE: The inverting of the Resolver / Encoder feedback counts outlined in an early step can affect operation throughout troubleshooting. If your motor does not run properly during one of the tests, make sure to invert parameter again before continuing with remaining tests (try subsequent tests with, and without, inverting the counts).

[QuickLink for the 890 on Parker.com] - Manual, QuickStarts, Product Support, etc

[QuickLink for the 890PX on Parker.com] - Manual, QuickStarts, Product Support, etc

4SEP19 JD

update 6JAN2023 JD

  • configure
  • PMAC
  • permanent magnet
  • startup
  • troubleshoot
  • commutation
  • commutate
  • 890
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply