Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Parker Motion Manager: What's New or Different Compared to ACR-View?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Parker Motion Manager: What's New or Different Compared to ACR-View?
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
  • -Motion and Machine Controllers
    • -ACR Controllers
      • -7000
        • ACR Binary Host Interface - 7000 and IPA
        • ACR7000 and IPA - AcroBasic PROGRAM SAMPLES
        • ACR7000 Connector part numbers
        • ACR7000 Controller differences to ACR9000
        • ACR74T Stepper Power Supply Sizing
        • ACR74V ACR78V: How to Reset BiSS Absolute Encoder Position
        • BE and SM Servo Motor Speed-Torque Curves at 24volts and 48volts
        • Expanded DEFINES allows numeric characters
        • Expansion I/O Information for ACR7000 and IPA
        • P Series Servo Motor Speed-Torque Curves at 24volts and 48volts
        • Parker Motion Manager Software Computer Requirements
        • Parker Motion Manager: What's New or Different Compared to ACR-View?
        • PC to ACR Program Samples (Excel, LabView, VB.Net, C++, C#)
        • Stepper Motor and Feedback Connectors
        • Time Saving Tip: Use Axis Copy if using same motor on other axes
        • Using #DEFINE inside PMM programs
      • +9000 (Legacy)
      • +IEC PLC (9600) (Legacy)
      • +PC Card Controllers (Discontinued)
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • +PAC120
    • +PAC340
    • +PAC320 (Discontinued)
    • +6K (Discontinued)
  • +General Technology Information
  • +Virtual Engineer
  • +Visualization and Human Machine Interface (HMI)
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • +AC and DC Drives and Inverters
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
  • What replaces the Gemini GV6K servo drive controller?

You are currently reviewing an older revision of this page.

  • History View current version

Parker Motion Manager: What's New or Different Compared to ACR-View?

Related FAQ:  ACR7000 Controller differences to ACR9000 

The ACR7000 family is supported by a new software tool, Parker Motion Manager (PMM). Parker Motion Manager combines the best of ACR-View and years of user feedback in a modern, user friendly and scalable software development environment. PMM is newly built and independent from ACR-View, allowing both software tools to be installed.

 New Features include:

  • Streamlined set-up Wizard
  • Product specific status panels
  • Improved terminal emulator
  • New-look Oscilloscope tools
  • Projects stored as single files for easy sharing and archiving

For ACR programmers new to Parker Motion Manager (PMM), many improvements have been implemented.  Layout is similar in terms of having a connection, configuration wizard, program editor, status panels. This summary is a brief synopsis of major differences between the two development packages.

Parker Motion Manager software is available for ACR7000 stepper product, which is a compact 4axis stepper drive controller.

PMM will be expanded in the future to support the IPA (single axis servo drive controller) but will not support ACR9000 (multi-axis controller). The latter isn't possible as the ACR9000 had many options (usb, serial, CANopen, EthernetPowerlink) that would be too large an undertaking. A new product is in development for 9000 applications; contact your local Parker ATC distributor.

1.  Both use ComACRserver which is installed with PMM or ACR-View6. If users have developed PC interfaces to the ACR9000 or IPA, these will work the same with the ACR7000.

2. When starting PMM users will immediately note Recent Projects allowing users to quickly jump in and get working. These are both on the optional Start Page and under File 

Default is 9 files and can be changed.

As comparison, ACR-View had a scroll list of projects but not sorted by last used.

3. Uploading from an existing controller is now easier from the New Project window  (File > New Project):

With ACR-View, users would have to create a new project, select the controller and then upload.

4. With Parker Motion Manager, projects are now stored as a single file (.pprj) making easier to transfer and share:

In ACR-View, projects were a folder with separate files for the .8k program, configuration, etc

5. In Parker Motion manager, System Code is generated every time on Finish. 

In ACR-View, it was generated as users moved through the Configuration Wizard which caused issues if users re-opened the project and jumped around in the different sections to edit/tune/adjust settings.

6. Terminal window changes:

Users can now arrow up and arrow down rather than re-type commands.  This much loved feature of power coders (from DOS windows of yester-year) is now available!

This is made possible as lines are now only sent when pressing enter. 

A. Dedicated buttons for jumping between programs, LIST program, LIST with line numbers and Clear display.

B. Expanded buttons on the right for common commands (5 groups of 12 user buttons)

C. Expanded User buttons with multiple lines 

D. The 4th and 5th group of buttons have been pre-populated with common commands.

Power users have full edit access and can re-use these groups but these pre-defined buttons help new users.

7. Defines is now in chart format making it easier for programmers to put in description for to name bits and parameters and constants.

8. Defines can be created directly from the Numeric Status panels by right-clicking:

9. PMM Windows can be docked, pinned or resized. This is a windows behavior Microsoft had expanded and evolved with .Net framework:

10. Configuration Wizard now includes Parker mechanics (actuators, precision tables and gearheads) for inches or millimeters.

This saves looking up the mechanics part numbering and catalog information to set the number of motor revs to in or mm

11.  Same motor on multiple axis?  Quickly populate the Configuration using Axis Copy (right-click on Axis):

12.  Testing code and want to remove a section of code (comment out multiple lines)?

Rather than typing REM or ' at the beginning of each line, select the lines and use the below highlighted icon on the tool bar.

This was a feature added into ACR-View6 but not older versions of ACR-View but nice time-saver:

13. In ACR-View when doing a Find, the first instance was found and then the focus was set on the program editor. So when users pressed enter, it would remove that instance (inserting an enter). 

In PMM, the focus reminds on the Find next window. So now when pressing enter, it'll move to the next instance allowing users to quickly move through the code instead of mouse clicking. Not a big change but a nice change for power users / heavy programmers. Yay!

14. Improved Servo Tuning screen and graphing!

Channel defaults set for standard motion tuning. Auto-Scaling so no more hunting. 

Easy motion! Set the distance & time and the move shape, with optional s-curving and motion is already generated automatically:

What's the values of all the channels at the same point in time? Just mouse over!

No need to export to Excel (though that's still available for power users).

15.  PMM File Transfer gives status during download.

Also will note highlight the errors:

16. Product specific status panels

17. Oscilloscope now has Bits available to graph

ACR-View had this function with a work-around but now users can easily select Bits to visually graph these changes compared to other bits/parameters in their programs.

18. 4 Watch windows now available. Each Watch list can hold 20 lines of bits or parameters. No more switching between Numeric / Bit Status!

To populate Watch list, within Motion Status Panel, right-click on indicators:

Or from the Numeric, Bit status or Defines, just right-click:

19.  User Parameters and User Bits are now in Numeric / Bit Status! Yay!

This includes user parameter p0 - p4095, and user non-volatile parameters (p39168 - p39423) and non-volatile longs (p38912 – p39167).

20. Invert direction on an axis is now easily done with a check box in the Configuration Wizard.

21. Save to Flash in ACR-View was 30-60sec. This has been greatly improved with PMM.

22.  New ease of use feature:  Zoom in Program editor:  hold Control key and use mouse scroll wheel to zoom in and out.

10/1/19 jh

12/3/19 jh added Axis Copy

1/8/20 jh added defines from numeric status,

1/13/20 jh added 12-14

7/31/20 jh added 15-20