Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How do I clone the AC10 with the 1002-00 module?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How do I clone the AC10 with the 1002-00 module?
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
  • AC/DC Industrial Drives-
    • AC10-
      • AC10 Heat Dissipation
      • AC10: Is the keypad detachable during operation?
      • AC10: Why am I getting over-voltage trips?
      • AC10: Why is my AC motor running hot?
      • Can I program through the keypad and DSELite on the AC10?
      • How can I configure an AC10 to run at two different speeds without using an analog input?
      • How do I connect an AC10 to a TS8000?
      • How do I clone the AC10 with the 1002-00 module?
      • How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and PDB?
      • How do I implement a Fast Stop circuit on the AC10?
      • How do I know what firmware revision my AC10 is?
      • How do I reset an AC10 back to factory defaults?
      • How do I reset the master password in an AC10?
      • How do I set up an AC10 for torque control?
      • In what type of package is the AC10 available?
      • What are the basic parameters to run an AC Induction motor from just the keypad?
      • What are the basic wiring connections of the AC10?
      • What are the environmental operating conditions for the AC10?
      • What are the minimum and maximum 3-phase input voltage ratings for the AC10?
      • What default configurations are available for the AC10?
      • What is the current overload rating for the AC10 drive?
      • What kind of I/O is available on the AC10?
      • What safety standards does the AC10 meet?
      • What software and communication cable are used for programming an AC10?
      • Why won't my AC10 run my motor?
      • AC10 Modbus-RTU Example to Interact Xpress HMI (XTA)
      • Can an AC10 run a PMAC motor?
      • How does the password protection feature work in the AC10 (via DSE Lite)?
      • How does the password protection feature work in the AC10 (via the keypad)?
      • Updated Control Terminal Torque Specifications for AC10 VFD’s
      • When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.
      • Where do I get the AC10's Modbus RTU / programming connector?
    • AC30+
    • DC590+ Series+
    • AC890 Series+
    • AC15/AC20+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
    • Constant Torque (CT) versus Variable Torque (VT) in VFDs
    • DSE890 and DSELite Ethernet Connection Port Numbers
    • ACxx scope tool problems with Windows 11
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
How do I clone the AC10 with the 1002-00 module?

Print Friendly and PDF

The way to simply and efficiently clone an AC10 is with the 1002-00 module.

The other way to "clone" is if you use the same 1002-00 module as a serial converter to save your AC10 template from/to a drive via DSELite; or with some other RS485 converter. If you require a serial converter, the 1002-00 is advised.

  • Using the 1002-00 as an RS485 converter
  • Using a generic RS485 converter

This FAQ assumes you have all of the small components that come with the 1002-00 part number for some potential reasons mentioned below. Parts that come with the 1002-00 part number and information on the module are below:

 

Important Notes:

  • If the password feature has been enabled on the drive, that will need to be entered in F100 before cloning (copying or loading) is allowed.  If you attempt to clone a drive that is currently under password protection, you will get alarm code Er73 on the drive's display.  If you try to load a cloned config into a drive that is currently under password protection you will also get alarm code Er73 on the drive's display.
  • To use the 1002-00 module as a cloning tool for a 22kw drive or smaller your firmware must be version 2.07 or greater. Parameter F105 is the firmware version. Verify the firmware version of the drive.
  • Several parameters in the drive must temporarily be set to default values (and then changed back to application-dependent values after loading them into the new drive).

  • If your AC10 has a green serial terminal you may connect the module directly into the drive (and the cable can be used to extend it, as shown below, if horizontal space next to the drive is limited). Old models of the IP20 drives, that were less than 22Kw, may not have a green serial port. If this is the case, you will be unable to clone the AC10 module as the other port is only used for external keypad use. You must manually take note of all parameters being used to reprogram your new drive.

  • The module requires +5V: If AC mains is NOT present (to internally provide control voltage) you must supply an external +5V signal with the extension cable and converter piece.
    • You can not plug the USB end into a PC and the other end into the drive to supply +5V (if you plug in the USB side, it will not work as a cloning module).
    • The cable when extended, and a pictorial description for the supply required without AC mains powering the drive are below:

   

AC10 Port Locations: 

  1. [IP20 < 22Kw]
  2. [IP20 > 22Kw]
  3. [All IP66]

    

Using the tool to clone:

To “COPY” the AC10 drive parameters into the Clone tool: .

  1. Slide the toggle switch into the "Unlock" position located on the side of the module.
  2. Press & hold the COPY ▲button until the drive display shows COPY. This may take 5 seconds. You may let go when you see "COPY".
  3. The C/U LED on the module will turn Red on then off.
  4. When the parameters have been downloaded successfully, the S/F LED will be Green.

If you get an alarm on the keypad showing Er73, password protection is currently enabled on that drive.

To “LOAD” parameters into an AC10 drive: 

  1. To copy Motor Parameters set F640 = 0. By default F640 = 1. Motor data is NOT copied. Click the table below to clarify it.
  2. Set the toggle switch to the "Locked" position.
  3. Press the LOAD ▼button. The drives display will show LOAD. This could take up to 10 seconds. You may let go when you see "LOAD"
  4. The C/U LED on the clone tool will turn Red on then go off.
  5. When the parameters have been downloaded successfully, the S/F LED will be Green.

The options when copy/loading Parameters (click for clarity):

  

If you get an alarm on the keypad showing Er73, password protection is currently enabled on that drive.

[QuickLink for the AC10 on Parker.com] - Manual, QuickStarts, Product Support, etc

14OCT19 JD

glh May 2022 added notes about password protection

  • 1002-00
  • guide
  • copy
  • AC10
  • parameters
  • cloning
  • clone
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply