Remedy: Be sure to use the SET statement to create the new oject.
Example: (also shows Ethernet connection)
Dim stat As BOXBRIDGELib.Status
Dim util As BOXBRIDGELib.Utility
Dim cntl As BOXBRIDGELib.Control
Set stat = New Status
stat.bOnConnectTest = False
stat.bstrIP = "192.168.10.40"
stat.Connect 3, 0
Set util = New BOXBRIDGELib.Utility
util.bOnConnectTest = False
util.bstrIP = "192.168.10.40"
util.Connect 3, 0
Set cntl = New BOXBRIDGELib.Control
cntl.bOnConnectTest = False
cntl.bstrIP = "192.168.10.40"
cntl.Connect 3, 0