Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base AC650 Series (Discontinued)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base AC650 Series (Discontinued)
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
  • AC/DC Industrial Drives-
    • AC10+
    • AC30+
    • DC590+ Series+
    • AC890 Series+
    • Legacy/Discontinued Products-
      • AC690+ Series (Discontinued)+
      • TS8000, DSI3, & DSI8000 (Discontinued)+
      • 5507 Analog Panel Meters (Discontinued)
      • AC584 Series (Discontinued)
      • DC590 Series (Discontinued)
      • AC620 Series (Discontinued)
      • AC650 Series (Discontinued)
      • What do I replace my AC650 drive with?
      • How can I connect to a 590C or 590D with DSE Lite?
      • L5392 Color LinkStation Information
      • Replacement LINK Fiber Optic Cable
      • What is DSD and LINK?
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • AC15/AC20
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
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
AC650 Series (Discontinued)

Print Friendly and PDF

The AC650 series is obsolete. It was an AC drive product tailored to V/Hz and Sensorless Vector operation. It was originally from the late 90s and it was subsequently replaced by the combined might of performance enhanced, modern products. Full obsolescence occurred in 2016 with the 650 Family Obsolescence Bulletin.

These drives are no longer supported unless assistance is required to migrate to a modern product. Your local Parker Distributor/Integrator can assist with modern product implementation.  Below is [non-proprietary] information that Parker EMN has on these products to act as a database.

650 Series

All variants (including V, G, S) have been obsoleted as of November 9th, 2016.

Unique variants of the third digit (65x) are also not available

  • 650 – “Original” drive. Operated in V/Hz mode only.
  • 650V – “Vector” drive had sensorless vector control built in (in addition to V/Hz mode).
  • 650G – Was a 650V drive in almost every aspect, but with performance enhancement traits tailoring it to China’s target market at the time. Primarily operated at slower speeds.
  • 650S – “Servo” was capable of sensorless vector PMAC control. Originally out of Europe.
    • Information was/is limited for this variant in North America. Support was limited in the US then, and is no longer available now.
  • 65x – “Unique” variants such as the “652-“. Originally out of Europe.
    • Documentation denoting these variants is limited in North America. Many were, and remain, proprietary to Parker Europe (EME) or their customers. Support was limited in the US then, and is no longer available now.

Product Code Breakdown

Product code breakdowns can be found in the manuals. For the sake of quick reference, we have the following snippets for most of the product codes over the years.

650 Product Codes

You may have a European part number (ie: 650-XXYYYYZZ-AAA…). The manuals and above snippets will breakdown these codes without issue. For deciphering these however we also have the following document to assist with quick reference for your 650’s power, amperage, and voltage ratings; as well identifying additional options your original 650 may have to assist in migrating to a modern product. [This document also denotes other European part numbers for other families as well].

Product Code Configurator

Replacements

There is no drop-in replacement for the 650 family.

Advisement: Please see this FAQ for replacement paths.  Your local Parker Distributor/Integrator can assist with modern drive implementation.

Spare Parts: There are no spare parts available for the series.

Variant Backup: If you already have a 650 drive on standby, and it happens to be a different variant than the one you're using then there is a chance your original configuration can be placed into the replacement using DSELite. This is not supported, as a migration to a modern product is advised.

  • Project and Firmware compatibility: 650 Series - Project and Firmware Compatibility
    • 650V Drive will accept 650G templates – Some parameters may need to be reconfigured
    • 650G Drive will accept 650V templates – Some parameters may need to be reconfigured
    • See below in “Software Info” for DSELite download and additional firmware notes.

Product Manuals and Info

Note: The manuals are major firmware dependent as more parameters and some functionality were added to later major revisions. 

Note: Manuals are also variation specific.

Base/Variant 650 Manuals

Base/Variant 650 Brochures & Catalogs

Software / Firmware Info

Software information can be found within the respective software environment’s help files. Any of the following software may have been used with your drive.

  1. CELite - OBX software. No longer supported.
  2. CE - OBX software. No longer supported.
  3. DSELite– Modern (free) software used to communicate to current products if not an old LINK product.
    1. Help files can be found when you right click any function block.
    2. DSELite can flash firmware on a 650, but it must be within the same major revision.
    3. Link to DSELite Download and Cable Required to Communicate to a 650.

Important Software Notes:

  • IMPORTANT V5 Control Board Note
  • You could not load different major revisions of firmware into other major revisions of drives due to hardware constraints (If your drive was originally v3, you could not download v5 firmware into it).
  • Earlier revisions of templates may be migrated and installed into recent revisions of firmware. Although the software may throw warnings, and although we do not support the process, it is possible if your program was not robust. We advise testing overall functionality of the machine before operation when taking an older template version and placing it into later revisions of firmware (ie in a swap-out scenario and the replacement is later firmware).

Legacy Appnotes

These are some Appnotes from internal servers. They are no longer supported. They are included for the sake of legacy information ONLY.

650V and 650G Appnotes

Miscellaneous Information

Much of this information can be found in the manuals. They are included here for legacy reference only and are no longer supported.

This includes 2D dimensional drawings, wiring diagrams for default templates, internal parameter connection diagrams for software, calibration steps, quick-starts, etc.

Accessories and Options Information

650_650V Special Options

Various Quickstarts

Miscellaneous

31OCT19 JD

15DEC2021 DCLIFFE -- Updated links to HTTPS.

650-aaaa-bbb-c   650/aaa/bbb/c/dd/e/ff/g/h   650G/xxxx/xxx/xxx   650G-aaaaaaaa-bbbbb-cc  650V-aa-bbb-dd-eeeee-ff-ggg-hh   650V/aaa/bbb/c/dd/e/ff/g/h   650V/xxx/xxx/xxx   650V-aaaaaaaa-bbbbbb-cc   650V-aaaaaaaa-bbbbb-cc   650V-aaaa-bb-c-d-e

    • SSD
    • 650G
    • Legacy
    • 650V
    • 650
    • 650S
    • Eurotherm
    • Share
    • History
    • More
    • Cancel
    • Sign in to reply