ACR_Excel_Arrays.zip Microsoft Excel using VBA to upload/download Arrays using the ComACRServer6
LabView Example.zip LabView2019 Sample using ComACRServer6
ComACRServer6_VBNet.zip VB.Net Sample using the ComACRServer6
ComACRServer6_CPP.zip C++ Sample using the ComACRServer6
ComACRServer6_CSS.zip C# Sample using the ComACRServer6
ComACRServer6_VB6.zip Visual Basic VB6 Sample using the ComACRServer6
Note the ACR communications server, the ComACRserver6, is installed with Parker Motion Manager (PMM).
It can also be installed separately on a PC without PMM though always good to have PMM to be able to connect to the 7000 and troubleshoot.