Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How do I start troubleshooting a 590+?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How do I start troubleshooting a 590+?
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
  • AC and DC Drives and Inverters-
    • AC10+
    • AC30+
    • AC690+ Series+
    • AC890 Series+
    • DC590+ Series-
      • How do I start troubleshooting a 590+?
      • What are the basic wiring connections required to run a motor, using the factory default drive?
      • How to Extract and Install Parameters to the 590+ Drive using DSE Lite
      • Why won't my motor run?
      • How can I make sure my DC motor does not have a problem with the Field Windings?
      • Why is my DC motor running hot?
      • 590+: Is the keypad detachable during operation?
      • Can I disable the field to run Brushed PMDC (Permanent Magnet DC motor) on a 590+?
      • Can I select between Manual Speed Reference and Line Speed Trim Setting for the same Analog Input?
      • Can you download a DSELite file into the drive when the drive is running?
      • How can I get the DSELite software the 590+ uses?
      • How can I make sure the motor will not start rotating until the speed pot is at 0?
      • How can I manually tune a 590+ drive to my motor?
      • How can I pre-trip "speed feedback" alarm before the drive trips?
      • How can I replace the control boards in 590+ Frame 1 and Frame 2 drives?
      • How can I set up a 590+ to be a field controller?
      • How can I upgrade a 590+ Frame 1 or 2 drive version 5.x or 7.x to version 8.x - Control Board and Configuration
      • How can the 590+ be programmed?
      • How can the drive configuration be reset to factory defaults?
      • How do I clone my 590+ Drive with the keypad?
      • How do I copy the configuration of one drive to another using the keypad?
      • How do I flash my 590+ drive to a newer Minor Revision of Firmware?
      • How do I know what firmware revision my 590+ is?
      • How do I set up a 590+ External Stack?
      • How to I configure the 590+ for Preset Speeds?
      • Is there anything I can check for a SEQ PRE READY alarm?
      • Modbus TCP/IP Addressing for the 590+ drive with the Ethernet Techbox
      • My DC590+ drive is displaying a Missing Pulse Alarm, what should I do?
      • The 590+ is enabled, but the main contactor doesn't close. Why?
      • Upgrading a control door from a 590 to a 590+
      • What accessories can be added to the 590+?
      • What analog and digital I/O is available on the 590+?
      • What are the Communication options for the 590+?
      • What are the communication settings for the 590+ for the P3 Port?
      • What are the differences between the 590 and 590+?
      • What are the minimum and maximum 3phase input ratings for the 590+?
      • What are the reference power supplies available to terminal connections on the 590+?
      • What are the types of Speed Feedback for the 590+?
      • What is the current overload rating for the 590+ drive?
      • What is the maximum operating altitude for the 590+?
      • What is the operating temperature for the 590+?
      • What safety standards does the 590+ meet?
      • What USB-serial adapter should I use?
      • Why does the drive fault to "Over-Voltage" after the drive is enabled?
      • Why does the drive fault to "speed feedback"?
      • Why does the drive fault to 3 phase-fail after the drive is enabled?
      • What I can I check for a CALIBRATION FAIL trip?
      • 590+ - Transferring a Configuration to a Drive with a Different Power Level
      • 598/599+ Stack Controller Replacements
      • DC590+ Encoder Feedback Card Options
      • DRV Contactor Options (955+ part numbers)
      • How do I convert DC590+ Europe part numbers to US part numbers?
      • Speed Regulation with 590+ Drives
      • Troubleshooting a DC brushed motor
      • What are differences between a Regen and Non-Regen 590+?
      • What does "NET FAIL" indicate in DSE Lite when using a LinkNet Techbox module on my 590+ drive?
      • Why is every light on the keypad flashing on my 590+?
    • TS8000, DSI3, & DSI8000+
    • Legacy/Discontinued VFD Products+
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
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
How do I start troubleshooting a 590+?

Print Friendly and PDF

     To get started, the 590+ manual has an extensive amount of troubleshooting assistance. If you are getting unwanted behavior or have a fault, then a dedicated section called "TRIPS AND FAULT FINDING" is a fantastic starting location to solving your problem. The manuals are thorough, and are firmware dependent. 

Manuals can be found on the 590+ on Parker.com under the "Product Support" tab. Accessory manuals (such as tech option cards) also have separate manuals associated with them.

Consult the manual for "Initial Drive Start" to ensure the drive is functioning properly and to get you started. Refer to "Calibration and Start-Up" chapter

Starting: "Trips and Fault Finding" section of the manual:

  1. Trips/Faults/Error Codes on the keypad. 
    1. There is an explanation of all trips and possible solutions to them in the manual that tech support will always have you try first.
  2. Flow-Chart Checklist Guides for:
    1. General operation
    2. Hardware troubleshooting
    3. Field failures
    4. Contactor failures
    5. SCR troubleshooting
    6. Motor checks
    7. etc.
  3. Alarm Status information as well as Diagnostics Information (both found through the keypad menu map, or in DSELite)
    1. Hexadecimal Representation of Trips - The LAST ALARM, HEALTH WORD, HEALTH STORE and ALARM HISTORY parameters use a four digital hexadecimal number to identify individual trips.  Each trip has a unique corresponding number as shown here
    2. You can see if there are other Alarms present
    3. If there are issues with parameters related to the issue
    4. Or find a pattern within the alarm history. 
    5. Note: It is common to see "Undervoltage" trips after power-down. Seeing "Undervoltage" during operation, is an issue.

After consulting the manual:

 Try checking out the FAQs in the sidebar under DC590+ Series to see if your issue has any write ups on it from an applications engineer.

  • If an article relevant to your issue is already posted, Parker Support would have you walk through it to gather more information or narrow down a root cause to start with.

After consulting the knowledgebase sidebar:

  1. Do you have the proper monitoring devices if relevant to the issue (Oscilloscope, current clamp, etc?)
  2. Are you able to narrow the issue down to one part of the machine?
    1. Have you tried swapping hardware if pertinent?
    2. Is one side of the machine working but another not?
    3. Is the drive getting proper signals from external sources? (Potentiometer, PLC, contactors, power supply, etc)
      • Example: Questions for a drive that does not want to start running from a fieldbus command would be:
        1. Is your PLC sending the proper control and status words?
        2. If so, is the drive accepting those parameters as viewable within DSELite?
        3. If further yes, then the issue may be programming logic not executing properly or you are missing various bits to send.
        4. If your PLC was not sending proper control and status words to begin with, check the PLC code.
  3. Use the DSELite software to view your programming. DSELite has Help files at the top of the window and within every function block to understand your specific programming and how it is executing.
    1. If no fault are on the keypad or in DSELite but you are getting unwanted behavior, you can extract the project file and then view it Online to see changes in real time with software debugging tools; or view how your specific machine's parameters are designed to interact.
    2. What Software and Communication Cable are used for Programming?
    3. How do I Extract Parameters from a 590+ to View Them?

    

21OCT19 15MAY20 JD

  • find
  • help
  • assist
  • code
  • fault
  • resource
  • troubleshoot
  • tips
  • manual
  • information
  • repair
  • course
  • 955+
  • 590+
  • inverter
  • Trip
  • control
  • 590P
  • broke
  • How
  • error
  • controller
  • guideline
  • damaged
  • info
  • fix
  • start
  • drive
  • 590
  • drv