To disable the 6K startup banner message, just address the unit to a non-zero value using the ADDR command. Only address zero will print out a startup banner message.
Example banner message:
*PARKER COMPUMOTOR 6K4 MOTION CONTROLLER
*NO REMOTE PANEL
To disable startup banner message:
ADDR1
*** This will disable banner messages on both communication ports on the 6K. ***
To enable start-up banner message:
ADDR0