Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Whats the difference between PIO-337 and PIO-347?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Whats the difference between PIO-337 and PIO-347?
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
  • -Motion and Machine Controllers
    • -ACR Controllers
      • +7000
      • -9000 (Legacy)
        • ACR9000 Family Letter of Volatility
        • ACR Gantry Lock and EPL Axes
        • ACR Homing Success/Failure Flags
        • ACR Order Code
        • ACR Servo Tuner - Move Back & Forth sample code
        • ACR-View 6 is frozen. How do I recover?
        • ACR-View Memory Dimensioning using the Oscilloscope
        • ACR9000 to ModuFlex connection pinout
        • Automating the EPL startup procedure
        • Can I use tools from ACR-View in my own PC application?
        • Compax3 and Aries Ethernet PowerLink I/O
        • Configuring Memory for ACR9000 Com Channels
        • Dual Loop with Analog Position Feedback
        • EPL Drive Enable Status
        • Free Online Training Videos: Parker ACR9000 programmable motion controller
        • Having problems connecting with USB - ACR View 6.0
        • How do I add PBOOT to PLC programs?
        • How much memory does my ACR controller have?
        • How to Read Compax3 Analog I/O with EPL SDO read?
        • How to connect ACR to PIO CANopen buscoupler?
        • How to disable RS232 autobaud for ACR9xxx
        • How to get status values from an Aries EPL Drive
        • How to read the absolute position from EPL drive?
        • How to select user units and axis scaling
        • INTCAP and MSEEK with Compax3 EPL
        • MSEEK EthernetPowerlink Compatibility
        • Memory Allocation for PLC programs
        • Output Reaction to EPL Failure
        • Remap CAN I/O for use with PLC
        • What is needed with various Parker I/Os?
        • What verison of the .Net Framework is needed for ACR-View 6?
        • Whats the difference between PIO-337 and PIO-347?
        • Where does ACR-View install the ComACRserver?
        • Why is controller reporting Program Stuck
        • 9000: Connector Part Numbers
        • ACR 9000 replacement: New ACR7000 series controller
        • ACR 9xx0 Recovering from Estop / Motion Enable input
        • ACR-View: Mapping a parameter to an oscilloscope channel
        • ACR9000 - CIP Communications stop on all devices when one CIP device goes offline
        • ACR9000 Ethernet Stream Connection Status Sample
        • ACR9000 Event Counters
        • ACR9000 Sample Input/Output Wiring
        • Are Parker IO modules available as NPN?
        • Connecting a Parker IO (PIO) to an ACR9000
        • EPL Velocity p38145 vs p8193 Master Velocity
        • Ethernet Communication Streams
        • Ethernet/IP Encoders
        • How do I set up Parker I/O (PIO)
        • How to command a home operation from HMI or PC app
        • Master Encoder for C3 EPL & ACR9040 system
        • Maximum USB Cable Length
        • Replacing the ACR9000 Battery
        • RS232 Electrical Noise on older 9000 Controllers
        • Senary Axis Flags
        • Updated EPL Network Flags and Parameters
        • Upload Absolute Position from a C3 to a ACR9000
      • +IEC PLC (9600) (Legacy)
      • +PC Card Controllers (Discontinued)
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • +PAC120
    • +PAC340
    • +PAC320 (Discontinued)
    • +6K (Discontinued)
  • +General Technology Information
  • +Virtual Engineer
  • +Visualization and Human Machine Interface (HMI)
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • +AC and DC Drives and Inverters
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
  • What replaces the Gemini GV6K servo drive controller?

You are currently reviewing an older revision of this page.

  • History View current version

Whats the difference between PIO-337 and PIO-347?

The PIO-337 is the standard CANopen bus coupler for the Parker-I/O system. A cheaper alternative is the PIO-347. The following table lists the differences between the PIO-337 "standard" and PIO-347 "econo" versions of this bus coupler.

StandardEcono

Total I/O bits supported51232
24V Fieldside Power SupplyYesNo*
No. of PDO32 Tx / 32 Rx5 Tx / 5 Rx
Device profileDS-401, programmable error response, marginal check, edge-triggered PDOsDS-401, programmable error response
DescriptionNo1No2
Input current500 mA260mA


In addition, the update rate of the PIO-347 is considerably slower than that of the PIO-337.

StandardEcono

Base Update Rate1 ms5 ms
Each Add'l Digital Point15 us100 us
Each Add'l Analog Point40 us270 us

* The PIO-347 requires the additional purchase of a PIO-602 Power Supply module