Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Can an AC10 run a PMAC motor?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Can an AC10 run a PMAC motor?
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
  • AC/DC Industrial Drives-
    • AC10-
      • AC10 Heat Dissipation
      • AC10: Is the keypad detachable during operation?
      • AC10: Why am I getting over-voltage trips?
      • AC10: Why is my AC motor running hot?
      • Can I program through the keypad and DSELite on the AC10?
      • How can I configure an AC10 to run at two different speeds without using an analog input?
      • How do I connect an AC10 to a TS8000?
      • How do I clone the AC10 with the 1002-00 module?
      • How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and PDB?
      • How do I implement a Fast Stop circuit on the AC10?
      • How do I know what firmware revision my AC10 is?
      • How do I reset an AC10 back to factory defaults?
      • How do I reset the master password in an AC10?
      • How do I set up an AC10 for torque control?
      • In what type of package is the AC10 available?
      • What are the basic parameters to run an AC Induction motor from just the keypad?
      • What are the basic wiring connections of the AC10?
      • What are the environmental operating conditions for the AC10?
      • What are the minimum and maximum 3-phase input voltage ratings for the AC10?
      • What default configurations are available for the AC10?
      • What is the current overload rating for the AC10 drive?
      • What kind of I/O is available on the AC10?
      • What safety standards does the AC10 meet?
      • What software and communication cable are used for programming an AC10?
      • Why won't my AC10 run my motor?
      • AC10 Modbus-RTU Example to Interact Xpress HMI (XTA)
      • Can an AC10 run a PMAC motor?
      • How does the password protection feature work in the AC10 (via DSE Lite)?
      • How does the password protection feature work in the AC10 (via the keypad)?
      • Updated Control Terminal Torque Specifications for AC10 VFD’s
      • When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.
      • Where do I get the AC10's Modbus RTU / programming connector?
    • AC30+
    • DC590+ Series+
    • AC890 Series+
    • AC15/AC20+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
    • Constant Torque (CT) versus Variable Torque (VT) in VFDs
    • DSE890 and DSELite Ethernet Connection Port Numbers
    • ACxx scope tool problems with Windows 11
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
Can an AC10 run a PMAC motor?

Print Friendly and PDF

Despite documentation and dedicated parameters that allude to PMAC control being possible (e.g. F106 - Control Mode), the AC10 is not suited for running a PMAC motor. It is still a completely viable option for AC induction motors in V/Hz or SLV mode.

Overall autotune behavior, which is required for a PMAC to be ran, is not optimized for PMACs. If the autotune does not fail outright on Overload or Overcurrent, it will continuously spin the motor indefinitely at high current (potentially burning the motor up if not stopped). Without an autotune, a PMAC motor can not be ran on a VFD. Part of the explanation for this is the motor poles parameter (F804) is directly tied to the motor's rated speed (F805) and unable to be changed independently. Normally, for AC induction motors, this is no issue as the pole count directly correlates to the base speed.PMAC features on the AC10 were designed around now-obsolete motors where the pole count and nominal RPM values followed that of AC Induction motors. (2 pole = 3600RPM, 4 pole = 1800 RPM, etc). For PMAC motors on the market these days, this is not the case; RPM and pole counts can vary widely.

Parker does offer alternatives:

  • For servo applications in general, we advise products that are tailored to PMAC control (all closed loop). Our Compax3 line as a great start.
  • For SLV PMAC control, consider our AC30 line.
    • Note the 890 is capable of PMAC control in closed loop vector mode, but is also not suited for sensorless vector PMAC control.
  • PMAC
  • AC10
  • sensorless
  • control
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply