The specific autotune procedure of a drive depends on the drive type and is simply guided in the drive's respective manual or quickstart guide. Both documents can be found underneath the "Product Support" tab on the respective product page, links provided below:
Parker.com/emn --> Drives and Inverters -->
What does it generally do, why do I need to do it?
The autotune is designed to "pair" a given drive and motor together. The autotune calculates some motor parameters and sets various gains in order to run the motor properly. The help files within the drive software (the provided Autotune function block, within each drive's specific template), software reference, and manual will all outline what parameters are calculated in an autotune. It does depend upon the drive type.
Importantly:
- AC10, 690+, 890, AC30, etc
- Required for Sensorless Vector and Closed Loop Vector modes. Not required in V/Hz mode.
- It is a rotating autotune for best performance, but a stationary autotune can be conducted if you have a documented value for the motor's magnetizing current.
- Required for Sensorless Vector and Closed Loop Vector modes. Not required in V/Hz mode.
- 590+, etc
- Required to run a motor properly for all modes of operation (armature voltage feedback, encoder, tachometer, etc).
- It is a stationary autotune. The shaft must be locked into place and not rotate.
- Required to run a motor properly for all modes of operation (armature voltage feedback, encoder, tachometer, etc).
Troubleshooting Faults after Auto-Tune
20DEC19 JD
17MAY22 JH Added Troubleshooting