Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Using JOG commands with AXIS identifier
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Using JOG commands with AXIS identifier
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)-
        • Free Online Training Videos: Parker AcroBasic - Programming Basics
        • ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample
        • AcroBasic program does not wait
        • ACR Binary Parameter Access Examples
        • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
        • ACR Memory usage and commands
        • AcroBasic Program Priority and Timing
        • Axis Flag update rate
        • Change axis positive/negative motion direction
        • Clear all memory in an ACR controller
        • Command Syntax for Variable Substitution
        • Commenting AcroBASIC Programs
        • Concerns when using DWL in programs
        • Concerns when using INH in programs
        • Creating Watchdogs for Ethernet Connections
        • Encoder Velocity
        • Error 17000 when attempting to communicate to ACR
        • Evaluation Underflow error
        • Evaluation overflow is line xxx
        • Hardware Position Capture for Encoder 8 and 9
        • Homing Application Note for ACR7xxx/ACR9xxx Controllers and IPA Drives
        • How can I check the axis PPU setting?
        • How do I set the frequency in an ACR SINE move?
        • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
        • How fast is my servo axis moving?
        • How to Calculate the Gear Offset Parameter?
        • How to Find Torque or Current commanded from ACR
        • How to home to a limit in AcroBasic
        • How to receive ASCII data
        • How to retrieve the raw SSI position from encoder?
        • How to Simulate Motion (without drives or motors)?
        • How to use CAM ON when source is moving
        • How to use the In Motion Bit
        • INT command not working properly
        • INTCAP
        • Is the ComACRsrvr thread safe?
        • LISTEN / LRUN - How to see line numbers
        • Output on Position Toggle Mode
        • PID Parameters when using Steppers
        • Position to a Torque / Current Mode
        • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
        • prohibited names for Axis aliases
        • Range Error on download for IF ENDIF statements
        • Range Error when commanding long moves - Distance limit 2^31
        • Reboot in startup program
        • Stopping motion in ACR controllers
        • System Pointer Address of ACR Global Variables, P0-P4095
        • Use of AXIS format
        • User Variables
        • Using ACR7xxx or ACR9xxx or IPA with LabView
        • Using CAM with PPU in user units (not counts)
        • Using Encoder 8 or 9 as SRC
        • Using JOG commands with AXIS identifier
        • Using an encoder or analog input as JOG SRC
        • Variable data types and transfer to AB plc via Ethernet/IP
        • VB generates Runtime Error 91 (accessing through the ACR Comm Server)
        • What ACR Global variables should I use in HMI applications?
        • What is the Binary Host Interface
        • What is the axis velocity
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Using JOG commands with AXIS identifier

Print Friendly and PDF

An axis can be jogged outside of the program it is attached. When used outside the program, the axis name cannot be used; the axis must be referred to by the "AXIS n" identifier where "n" is the axis number.

Example
Axis 0 is attached to Program 0 using the configuration wizard and given the axis name "X". In program 0 or at the P00> prompt, the axis can be referred to by X:

JOG FWD X
JOG INC X -10
JOG ABS X 25
JOG OFF X


When another program is used to control jogging, AXIS 0 must be used instead of X (notice that the axis identifier has moved to the front of the command):

AXIS 0 JOG FWD
AXIS 0 JOG INC -10
AXIS 0 JOG ABS 25
AXIS 0 JOG OFF


NOT RECOMMENDED!! AXIS 0 can be placed after the JOG commands, this can lead to syntax errors (which is why the correct syntax is illustrated here) and confusing code:

JOG FWD AXIS 0
JOG INC AXIS 0 (-10)
JOG ABS AXIS 0 (25)
JOG OFF AXIS 0
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply