Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base PSD Software - PSD BRAKE CONTROL FUNCTION BLOCK
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base PSD Software - PSD BRAKE CONTROL FUNCTION BLOCK
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive-
      • Link to PSD Support Page
      • PSD Software - PSD BRAKE CONTROL FUNCTION BLOCK
      • PSD Software - Why are the help files in PSD ServoManager not displaying?
      • Resetting the Configuration (X60) Port IP Address in the PSD
      • Setting / Changing the Configuration (X60) Port IP Address in the PSD
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
PSD Software - PSD BRAKE CONTROL FUNCTION BLOCK

Print Friendly and PDF

At this time the PSD does not support the SMC3_BrakeControl Function Block.  The attached function block "PKR_PSD_BrakeControl" allows for manual control of the motor's mechanical brake when the PSD is in the DISABLED or ERRORSTOP brake.

The following is a description of the Function Block Operation:

     Function Block:  PKR_PSD_BrakeControl
     Date:                    2020.03.27
     Version:               01.00    - Initial Release
     Description:        This function block allows for MANUAL CONTROL of the PARKER PSD1 Series Servo Drive AXIS
                                   Mechanical Motor Brake.  By use of this function block in the application the motor brake can be
                                   OPENED when Axis1 is in the DISABLED or ERRORSTOP State.  Otherwise, control of the Mechanical Brake
                                   is handled AUTOMATICALLY when the drive is ENABLED or DISABLED using MC_POWER.  The Function Block
                                   does not take on any further monitoring or other intelligent functions (i.e. time delayed opening of
                                   the brake).

                                   Function Block Errors are cleared when bExecute goes FALSE.  Error Codes and Error Messages defined as follows:

                                   dwErrorID 0    - PKR_NO_ERROR
                                   dwErrorID 1    - PKR_DRIVE_ENABLED
                                   dwErrorID 2    - PKR_ETC_WRITEPARAMETER_COE_ERROR
                                   dwErrorID 3    - PKR_DRIVE_ENABLED_DURING_FB_EXECUTION

The Function Block can be added to a PAC or CODESYS project by importing the function block into the selected Application within the Devices window or by importing it into the POUs Window. 

PKR_PSD_BrakeControl.zip

  • PAC
  • PAC FUNCTION BLOCKS
  • PSD FUNCTION BLOCKS
  • PSD
  • FUNCTION BLOCKS
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply