Parker Motion Manager (PMM) is the software development environment for creating project configurations and AcroBasic programs for the ACR7000 series controllers and integrated multi-axis drive controllers (servo and stepper) and the Intelligent Parker Amplifier (IPA).
ParkerMotionManager_InstallationRequirements.pdf
Installation Permissions
If installing software that uses Microsoft Access Database Engine 2007 such as InteractX, this will cause PMM to stop working. To fix, uninstall PMM and Access Database Engine 2010 and then re-run the PMM installer. This will re-install the database engine and PMM. PMM installer includes Visual C++ redistributable and Access Database Engine and do not need to be manually installed nor downloaded. If already installed on the PC, these steps will be skipped.
Security software may block installation of PMM and the redistributables. Users will need permissions to install software. An example of this is Beyond Trust computer management. Microsoft's User Access Control through company IT policies may also may block software installation.
in process
32 Bit vs 64 Bit
Parker Motion Manager uses 32bit Access Database Engine.
If users need 64bit version of Parker Motion Manager, contact support at emn.service@support.parker.com
Keywords: ACR74T ACR74C ACR78C ACR74V ACR76V ACR78V ACR7900
Windows Win7 Windows7 Win10 Windows10 PC
ACR7000 Controller http://www.parkermotion.com/products/Controllers__7329__30_32_80_567_29.html
ACR7000 Stepper http://www.parkermotion.com/products/Stepper_Drive_Controllers__7329__30_32_80_567_29.html
ACR7000 Servo http://www.parkermotion.com/products/Servo_Drive_Controllers__7329__30_32_80_567_29.html
IPA Servo http://www.parkermotion.com/products/Servo_Drive_Controllers__7313__30_32_80_567_29.html
4/10/20jh
12/20jh Note about 2007 Access Database Engine added.