Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Parker Motion Manager Software Computer Requirements
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Parker Motion Manager Software Computer Requirements
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
  • -Motion and Machine Controllers
    • -ACR Controllers
      • -7000
        • ACR Binary Host Interface - 7000 and IPA
        • ACR7000 and IPA - AcroBasic PROGRAM SAMPLES
        • ACR7000 Connector part numbers
        • ACR7000 Controller differences to ACR9000
        • ACR74T Stepper Power Supply Sizing
        • ACR74V ACR78V: How to Reset BiSS Absolute Encoder Position
        • BE and SM Servo Motor Speed-Torque Curves at 24volts and 48volts
        • Expanded DEFINES allows numeric characters
        • Expansion I/O Information for ACR7000 and IPA
        • P Series Servo Motor Speed-Torque Curves at 24volts and 48volts
        • Parker Motion Manager Software Computer Requirements
        • Parker Motion Manager: What's New or Different Compared to ACR-View?
        • PC to ACR Program Samples (Excel, LabView, VB.Net, C++, C#)
        • Stepper Motor and Feedback Connectors
        • Time Saving Tip: Use Axis Copy if using same motor on other axes
        • Using #DEFINE inside PMM programs
      • +9000 (Legacy)
      • +IEC PLC (9600) (Legacy)
      • +PC Card Controllers (Discontinued)
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • +PAC120
    • +PAC340
    • +PAC320 (Discontinued)
    • +6K (Discontinued)
  • +General Technology Information
  • +Virtual Engineer
  • +Visualization and Human Machine Interface (HMI)
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • +AC and DC Drives and Inverters
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
  • What replaces the Gemini GV6K servo drive controller?

You are currently reviewing an older revision of this page.

  • History View current version

Parker Motion Manager Software Computer Requirements

Parker Motion Manager (PMM) is the software development environment for creating project configurations and AcroBasic programs for the ACR7000 series controllers and integrated multi-axis drive controllers (servo and stepper) and the Intelligent Parker Amplifier (IPA).

ParkerMotionManager_InstallationRequirements.pdf

If installing software that uses Microsoft Access Database Engine 2007 such as InteractX, this will cause PMM to stop working. To fix, uninstall PMM and Access Database Engine 2010 and then re-run the PMM installer. This will re-install the database engine and PMM.  PMM installer includes Visual C++ redistributable and Access Database Engine and do not need to be manually installed nor downloaded.  If already installed on the PC, these steps will be skipped.

Security software may block installation of PMM and the redistributables. Users will need permissions to install software. An example of this is Beyond Trust computer management. Microsoft's User Access Control through company IT policies may also may block software installation.

Keywords: ACR74T ACR74C ACR78C ACR74V ACR76V ACR78V ACR7900

Windows Win7 Windows7 Win10 Windows10 PC

ACR7000 Controller  http://www.parkermotion.com/products/Controllers__7329__30_32_80_567_29.html

ACR7000 Stepper http://www.parkermotion.com/products/Stepper_Drive_Controllers__7329__30_32_80_567_29.html

ACR7000 Servo  http://www.parkermotion.com/products/Servo_Drive_Controllers__7329__30_32_80_567_29.html

IPA Servo  http://www.parkermotion.com/products/Servo_Drive_Controllers__7313__30_32_80_567_29.html

4/10/20jh

12/20jh Note about 2007 Access Database Engine added.