Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)+
    • InteractX+
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
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
Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.

Print Friendly and PDF

The suspended issue is due to an incomplete install probably when the installer ran into a problem it bailed.

To fix that, it needs to be removed from the installer data Windows stores so it can do an uninstall of software. To do that:

Go to the folder shown below, make a Hold folder and MOVE all of the folders into it:

Then it will allow the installer to run again. After the installation completes, move all the folders back and it will stop and say one of the folders all ready exists. This will be the InteractX folder so say no. That keeps the bad install folder in the hold folder which you can then delete.

One thing that Windows 10 might be missing is the .net frameworks since it is now an option that needs turned on not installed. Turn this on for Windows 10 units as shown on the Microsoft site shown below.

DM06042020

  • Install
  • Windows 10
  • Windows 7
  • InteractX
  • Uninstall
  • Installshield
  • Interact Xpress Manager