You can use these spreadsheets to convert AC890 part number formats.
Step 1 - Open the file below that corresponds to the first several characters of the UK European/JDE part number you wish to convert. For example, if the part number begins "890SD-43", open the file named 890SD-43... 890 Drives 460V.xlsx
Step 2 - Edit the green shaded fields using the drop-down menus as per the part number you want to cross over. If prompted for a password the first time, it's ID10T. As you finish entering the part number, the US part number will populate in the yellow cells, along with useful notes.
890SD-23 890CD-23... 890 Drives 230V.xlsx
890SD-43... 890 Drives 460V.xlsx
890SD-53... 890 Drives 500V.xlsx
890CD-43... 890 Drives 650VDC.xlsx
890CD-53... 890 Drives 650-705VDC.xlsx
890CA 890CS... 890 Common Adapter & Common Supply r1.xlsx
FAQ: How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?