Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Range Error when commanding long moves - Distance limit 2^31
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Range Error when commanding long moves - Distance limit 2^31
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)-
        • Free Online Training Videos: Parker AcroBasic - Programming Basics
        • ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample
        • AcroBasic program does not wait
        • ACR Binary Parameter Access Examples
        • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
        • ACR Memory usage and commands
        • AcroBasic Program Priority and Timing
        • Axis Flag update rate
        • Change axis positive/negative motion direction
        • Clear all memory in an ACR controller
        • Command Syntax for Variable Substitution
        • Commenting AcroBASIC Programs
        • Concerns when using DWL in programs
        • Concerns when using INH in programs
        • Creating Watchdogs for Ethernet Connections
        • Encoder Velocity
        • Error 17000 when attempting to communicate to ACR
        • Evaluation Underflow error
        • Evaluation overflow is line xxx
        • Hardware Position Capture for Encoder 8 and 9
        • Homing Application Note for ACR7xxx/ACR9xxx Controllers and IPA Drives
        • How can I check the axis PPU setting?
        • How do I set the frequency in an ACR SINE move?
        • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
        • How fast is my servo axis moving?
        • How to Calculate the Gear Offset Parameter?
        • How to Find Torque or Current commanded from ACR
        • How to home to a limit in AcroBasic
        • How to receive ASCII data
        • How to retrieve the raw SSI position from encoder?
        • How to Simulate Motion (without drives or motors)?
        • How to use CAM ON when source is moving
        • How to use the In Motion Bit
        • INT command not working properly
        • INTCAP
        • Is the ComACRsrvr thread safe?
        • LISTEN / LRUN - How to see line numbers
        • Output on Position Toggle Mode
        • PID Parameters when using Steppers
        • Position to a Torque / Current Mode
        • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
        • prohibited names for Axis aliases
        • Range Error on download for IF ENDIF statements
        • Range Error when commanding long moves - Distance limit 2^31
        • Reboot in startup program
        • Stopping motion in ACR controllers
        • System Pointer Address of ACR Global Variables, P0-P4095
        • Use of AXIS format
        • User Variables
        • Using ACR7xxx or ACR9xxx or IPA with LabView
        • Using CAM with PPU in user units (not counts)
        • Using Encoder 8 or 9 as SRC
        • Using JOG commands with AXIS identifier
        • Using an encoder or analog input as JOG SRC
        • Variable data types and transfer to AB plc via Ethernet/IP
        • VB generates Runtime Error 91 (accessing through the ACR Comm Server)
        • What ACR Global variables should I use in HMI applications?
        • What is the Binary Host Interface
        • What is the axis velocity
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Range Error when commanding long moves - Distance limit 2^31

Print Friendly and PDF

Users cannot command a single distance move that crosses 2^31 (2,147,483,648)  the rollover point.

Two potential work arounds:

You can command a JOG FWD or JOG REV (continuous moves) across that threshold and then monitor the position register.

 

Or, you can however get around this with commanding it as 2 different moves without stopping.

So if you wanted to do 1000 incremental move and the PPU was large (such as a motor with high resolution absolute encoder and/or with high gear ratio):

 

STP 0

Y/500

STP 10

Y/500

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply