Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Flash Player Ongoing Support in Xpress 4.2 and Parker Remote Browser
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Flash Player Ongoing Support in Xpress 4.2 and Parker Remote Browser
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
  • +Motion and Machine Controllers
  • +General Technology Information
  • +Virtual Engineer
  • -Visualization and Human Machine Interface (HMI)
    • +Interact (Legacy)
    • +InteractX
    • -Interact Xpress
      • Interact Xpress Misc - How to Flashback Compact Flash (CF) Card for Parker HMIs
      • Device Read Error with MicroLogix
      • Flash Player - Parker Remote Browser compatibility issues with the older versions of Xpress
      • Interact Xpress C3 Error History Display
      • INTERACT XPRESS HOW TO ORDER
      • Interact Xpress Manager - Troubleshooting - Ver 4.2 Error Flash Player not installed
      • Interact Xpress Misc - Are all tags written all the time? Where to set this?
      • Interact Xpress Misc - Can I send an Alarm E-mail to more than one person?
      • Interact Xpress Misc - Creating New Projects for older versions of Xpress using Seed Projects in Xpress Manager 4.x
      • Interact Xpress Misc - How can I find out what TCP/UDP ports my software is using?
      • Interact Xpress Misc - How do I get through my router for remote Interact Xpress panel access?
      • Interact Xpress Misc - How to change the sort order for recipes in Xpress?
      • Interact Xpress Misc - Loading Xpress Application on the XPR on bootup
      • Interact Xpress Misc - Test PLC driver connection setup BEFORE downloading to the HMI - If the Development PC can not talk to PLC, the HMI won't ether.
      • Interact Xpress Misc - Updating the Firmware (Xpress version) on the Xpress HMI Hardware
      • Interact Xpress Misc - Updating Xpress Project Versions & Creating Backup Copy
      • Interact Xpress Misc - User Configurable Driver User Guide (UCON)
      • Interact Xpress Misc - What can I do if I don't know the Xpress Admin Password?
      • Interact Xpress Misc - What size Compact Flash card is supported by XPR/XPC?
      • Interact Xpress Misc - Where is the driver documentation and tag format information?
      • Interact Xpress Misc - Which HMI runs Interact Xpress?
      • Interact Xpress Misc - Which Xpress Version works with my? XPR / XPR2 / XT
      • Interact Xpress Misc - XPC2, XPR2 and EPX2 PowerStations no longer include audio hardware (SB975)
      • Interact Xpress Misc - XPR/XPR2 Flashback Utilities
      • Interact Xpress Misc - XPR/XPR2/XTA Setting the System Time, IP address, Touchscreen Calibration require access to the Xpress Shell Screen but Application has no Exit Button
      • Interact Xpress Misc - Xpress Flashback for XTA and required Memory Card.
      • Interact Xpress Misc - Xpress Manager Archive
      • Interact Xpress Misc - Xpress Time and Date Tags and how they are related and used to set the HMI system Time and Date
      • Interact Xpress Software - Control Access to Panels and Tools using the Password User Levels in Xpress / Embedded Xpress (PAC)
      • Interact Xpress Software - How do I control the Lens States for an Indicator tool in Interact Xpress?
      • Interact Xpress Software - How do I set a value to my device from my Xpress panel only when a button is pressed?
      • Interact Xpress Software - How do I write/read strings between Xpress (XPR) and ACR?
      • Interact Xpress Software - How to switch screens from a PLC
      • Interact Xpress Software - How to wrap text on a tool in Xpress Manager?
      • Interact Xpress Software - Xpress Recipe Naming
      • Interact Xpress Training - AB ControlLogix Ethernet Communication Driver - Manual Creation of Controller (Global) Atomic Tags in Xpress Manager
      • Interact Xpress Training - AB ControlLogix Ethernet Communication Driver - Manual Creation of Program (Local) Atomic Tags in Xpress Manager
      • Interact Xpress Training - AB ControlLogix Ethernet Driver - Manual Creation of Controller (Global) STRING Tags in Xpress Manager
      • INTERACT XPRESS TRAINING - AB CONTROLLOGIX ETHERNET DRIVER - MANUAL CREATION OF PROGRAM (LOCAL) STRING TAGS IN XPRESS MANAGER
      • Interact Xpress Training - Importing Tags into Xpress from Control Logix / Compact Logix
      • Interact Xpress Training - Interact Xpress with Parker-SSD AC890 Drive Products
      • Interact Xpress Training - Tag Rules (Tag Sharing) Examples
      • Interact Xpress Training - Using with Compax3 for Torque Control (Example)
      • Interact Xpress Troubleshooting - Auto E-Mail on Alarm activity not working with Free E-mail servers
      • Interact Xpress Troubleshooting - CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Interact Xpress Troubleshooting - Fonts unreadable on tools or animations broken after upgrading 2.16 and older Projects to 3.1 or 4.1
      • Interact Xpress Troubleshooting - If losing connection to PLC, turn on Auto-Demotion
      • Interact Xpress Troubleshooting - IOCTL NDIS REBIND ADAPTER error on XT
      • Interact Xpress Troubleshooting - Messages disappear from Multi-State indicator after application closed and re-opened when & is used in message
      • Interact Xpress Troubleshooting - My Xpress projects disappeared after I upgraded my Pre-2.1.6 version to 2.1.6 or higher
      • Interact Xpress Troubleshooting - My Xpress version did not change when I did an upgrade to the latest version on my development PC
      • Interact Xpress Troubleshooting - Not able to add tags in Tag Editor using (New Tag)
      • Interact Xpress Troubleshooting - Step 3 Error when clicking Design in your Xpress Project
      • Interact Xpress Troubleshooting - UCON Floating point values have Commas where the Decimal point should be
      • Interact Xpress Troubleshooting - Workaround for getting flash to work on Android 4.0xxx revs
      • Interact Xpress Troubleshooting - XPR / XPR2 Flash Player error dialog pop-up (long running script....) or screen stops updating.
      • Interact Xpress Troubleshooting - Xpress Manager / Unable to Exit Runtime or Designer running on Windows 10
      • Interact Xpress Troubleshooting - Xpress Manager crashes when importing a JPG
      • Interact Xpress Troubleshooting - Xpress Manager Menus clipped/chopped off. Setting size to Small/Medium/Large does not change the viewable menu.
      • Interact Xpress Troubleshooting - XT replacement panel won't connect over ethernet
      • Modbus Device Compatibility with InteractX and Interact Xpress
      • Parker Remote Browser -- Connect to Xpress HMI at Startup
      • Xpress 4.2 install OCX failed to register and the Xpress Manager "Help - About IXM " shows blank Flash player version.
    • +IXA / PCA
    • +IPX / IPC (Discontinued)
    • +PHM / PM1 Industrial Monitors (Discontinued)
    • +PA / PS / P1-P9 (Discontinued)
    • +PX / HPX InteractX HMIs (Discontinued)
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • +PFD - Parker Factory Display (Discontinued)
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +AC/DC Industrial Drives
  • +Gearheads
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)

You are currently reviewing an older revision of this page.

  • History View current version

Flash Player Ongoing Support in Xpress 4.2 and Parker Remote Browser

Flash Player Support - Xpress, PFD and PAC Embedded Xpress Remote Browsing

Adobe and Microsoft have terminated support for Flash Player as of December 31, 2020

This will affect the Development side of Xpress (Xpress Manager) and browsers used to access HMIs remotely. (IE, Chrome, Firefox etc...)

The browsers require plug-in software from Adobe to play Flash content and these plug-ins are being actively removed by Microsoft and the Browsers.

Will the Runtime HMIs stop working?

No. The Runtime HMIs are not affected by the Adobe EOL. They use embedded images that have Flash built in and will continue to work with no upgrades required.

Xpress Development PCs will be affected differently depending on the Windows OS, Browser used and Xpress Version.

All Windows 10 users that are getting regular Windows Updates will see immediate problems with Xpress Manager and Browsers for remote access.

If you are running older Windows versions and have Adobe Flash Player loaded and working, it will continue to work as long as no updates take place that delete Flash Player.

Accordingly, Virtual machines are not affected unless updated and the Flash Player removed or deactivated.

 

Parker has two new products to address the ongoing support of our Flash Based HMIs.

Xpress Manager 4.2 

Xpress Manager 4.2 version now includes a Parker Flash Player solution built-in which does not require Adobe Flash plug-in software.

Xpress Manger 4.2 natively generates Xpress 4.1 runtime files for use on the XTA so there is no upgrade necessary to the HMI.

Xpress Manager 4.2 can also open and edit any prior version Xpress Project without changing the version.

If you open a 3.1 project and do not upgrade, it opens the 3.1 editor and saves all edits as 3.1 version.

If you need to create a new project from scratch for a customer using the XPR or XPR2 and do not have an existing project, See this FAQ for Seed projects and instructions.

Click the Link to be directed to the Seed Projects FAQ.    Xpress SEED Projects.

 

Parker Remote Browser

The PRM uses the same PARKER SPECIFIC Flash Player technology as Xpress Manager 4.2 and provides remote viewing and editing access.

The Parker Remote Browser (PRM) does not rely on the downloaded Adobe Flash Player and works with Windows XP/7/10

Using the new Parker Remote Browser (PRM) will be very familiar as it works very much like all other web browsers.

It is just a streamlined version since it will only be used with the Parker HMIs.

To connect to the remote HMI, the IP address can be entered in the Home screen URL box or directly on the Web Address bar at the top.

PRM is a "Tabbed" type browser which can have multiple units tabbed in the same screen or a new instance can be opened to have more units viewable at the same time.

PRM also supports Bookmarks allowing you to type in your IP address once and then bookmark the unit. Next time it can be started from bookmarks.

 

Important Notes:

This browser will only play Flash Player files that are part of the Parker Xpress, PFD and PAC.

It can not be used to access other Flash enabled programs or to run Flash Player SWF files alone

 

The Licensing for these new products prohibits downloading them from or using them in China.

 

PLACEHOLDER FOR DOWNLOAD LINK - In Process post by Jan 4, 2021

PLACEHOLDER FOR DOWNLOAD LINK - In Process post by Jan 4, 2021

12172020 dom