No. The magnets used are rare earth permanent magnets. They will only lose their strength if the temperature gets too high. This temperature, known as the Curie point, is about 100 C. Once this temperature is exceeded, the magnet will lose it's magnetic properties. Lowering the temperature will not result in gaining these magnetic properties back.