Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Motion Sizer: No motor/gearhead/actuator database error (No TS torque, Divide by 0)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Motion Sizer: No motor/gearhead/actuator database error (No TS torque, Divide by 0)
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
  • Other-
    • -E Motor Option
    • AC-03 / AC-07 / AC-10 / AC-15 manuals
    • Battery Replacement for 500 or JSI
    • C/CX Suggested Replacements
    • Cage Code
    • Changing the Configuration of the Compumotor Plus
    • Color Code for Stepper Motor External Encoder
    • Compumotor Plus motor internal potentiometers
    • Controller Cable Drawings
    • Custom Products
    • Daedal to Compumotor Cross Reference
    • Daisy chaining AR-C
    • DC Brushed Motor with the Aries & Gemini
    • Drive Input Power
    • Dumping the 3000 memory.
    • EDC TDC XDC VRP PMC
    • Encoder or Resolver?
    • Ferrite absorber
    • Heat Dissipation within Enclosures
    • How do I change the Btorq.dat file?
    • How do I download software from www.parkermotion.com?
    • How do I get support for my Parker SSD / Parvex division products?
    • How Much Power Do I Need?
    • Inertia Ratio
    • Is Parker Compumotor ISO9000 Certified?
    • KH/KS Error 62
    • KH/KS Motors
    • M-Drive/Motor Compatibility and Matching
    • Mating MS Connectors for KH motors
    • Motion Sizer: No motor/gearhead/actuator database error (No TS torque, Divide by 0)
    • My ARC-C or -D does not fit on my motor.
    • Obsolete Products -- 1990 - 1999
    • Obsolete Products -- 2000 and later
    • Offset voltage on the Compumotor Plus
    • Parker MotionSizer: Stationary Rack, Moving Pinion
    • Parker SBC Replacement products
    • PK130M Ordering Part Number Change
    • PK2 Part Number Change(5/9/97)
    • PMC Motion Controllers (PMC20 & PMC10)
    • Printing From Compumotor DOS-based Applications
    • QM Series Motor Information
    • Refurbished Inventory / Educational Discount
    • Setting the deadband on the VAC.
    • Smart Encoder Compatibility
    • Software for the SV
    • Three wire prox sensor color code
    • Torque Margin
    • Transformer Specs
    • Upgrading A/AX Systems
    • VM15 and VM25 Terminal Breakout Modules
    • What is a single and two speed resolver?
    • What is CE, EMC and LVD?
    • What is difference between CD35M and CD60/80M?
    • Windows 2000 locks up when printing
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
Motion Sizer: No motor/gearhead/actuator database error (No TS torque, Divide by 0)

Print Friendly and PDF

If Motion Sizer reports that it cannot locate the motor, Parker gearhead or Parker actuator databases, check the version MotionSizer for the version Windows first.

For Win10 or Win7-64bit use version 3.22.1040

For Win7-32bit or XP, use version 3.21.010D

If that's correct, then:

1. Uninstall Motion Sizer from computer's control panel.

2.  Locate Motion Sizer directory, by going into 'My Computer', and delete it. This directory is not deleted as part of the uninstall and prevents updating the databases.

For XP and Win7 32bit:
Default file location is: C:\Program Files\Parker\Parker Motion Sizer\

For Win7 64bit:
C:\Program Files (x86)\Parker\Parker Motion Sizer\

 

3. Re-Install Motion Sizer.

4. Do not open MotionSizer yet. Copy new databases that are included in the .zip download into MotionSizer directory. Old versions of the databases can be overwritten/replaced or deleted. See the readme.txt within the zip file.  This will need to be done for existing installations and after new installations.

5. Run MotionSizer as Admin. Go to Start menu > All Programs > Parker Hannifin. Right click on Parker Motion Sizer and select Properties...

 

 

6.  On the Compatability tab, select Run this program as an administrator and Apply.

 


You can verify that the motor databases are loaded correctly by clicking on 'Help', 'About', and seeing if there are version numbers next to the motor database names.

 

 

unknown original author.

5/16jh updated with Run as Admin, pictures, doesn't require restart PC

2/18 updated with versions for Windows. Download page updated.