Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Legacy Product Page - P1 Series
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Legacy Product Page - P1 Series
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
  • Visualization and Human Machine Interface (HMI)-
    • Interact (Legacy)-
      • Replace/Upgrade Interact panel P11/P1H/P15/P2/P3/P4/P5 etc
      • CTC and i-Motors
      • Configure a TCP/IP Dial-Up Adapter Connection.
      • Interact Misc - Can ASCII register in the PLC be used as an alarm?
      • Configure a TCP/IP connection (IP address)
      • Compact Flash Disk Transfer using Interact MachineShop Toolbar to Upload and Download
      • ERROR - Invalid Panel list or Key Pad Address.
      • Ethernet download to a CTC Panel.
      • How to Restore Motion Panel.
      • Interact Software - Display alarms in a RMD tool within PTM
      • How to run app on my PowerStation on boot-up?
      • Implementing the New CMOT Driver
      • LEDs on the back of the Profibus card
      • MachineLogic - How do I clear Retentive Memory?
      • MachineLogic - No project on the PLC.
      • Security Key Setup not Installed
      • Single layer SST 5136-PFB-104 card with Interact.
      • TCP/IP Ethernet and a Dial-Up Connection
      • TCP/IP open port failure
      • Can I run Interact 6.X in Windows NT/2K/XP?
      • Can I run Interact7 on my Windows 10 or 7 PC?
      • Configure a TCP/IP connection (DHCP)
      • Configure a TCP/IP direct Ethernet connection
      • CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Enable/disable the screen saver
      • Flashback Utilities for the CTC DOS Based PowerStations - If you have Interact ver 7 it installs all the necessary Flashbacks.
      • HMI Battery Replacements
      • How do I connect my P13, PA or PA2 Interact HMI to DataHighway Plus Network?
      • How do I recalibrate my Interact touchscreen? Or change the panel's ethernet address?
      • How do I show hidden and protected files in Windows?
      • How do I transfer my old Interact application to a newer Interact panel?
      • How to connect my device to Interact? Interact Cable Dictionary
      • How to print graphics from Interact run mode.
      • I upgraded my old hardware to a PA2 and have Vertical Stripes on screen and does not load my application.
      • Interact does not recognize the security key.
      • Interact: Error Initializing AMM - Invalid Logging Path
      • Minimum of NT 4.0 SP3 to install Machine Shop
      • Powerstation Shell on older CTC units
      • Replacing old HMIs that run Interact
      • Upgrading from a PA to a PA2
      • What are Interact Runtime modules?
      • Whats the difference between FLH-0512P and FLH-0512?
      • What internal variable can I use to R/W ASCII?
      • Interact Troubleshooting - WinXP- cannot select options on Toolbar
      • Control Access to Panels and Tools using the Password User Levels in Interact
      • Driver for my Allen Bradley Micrologix 1500 PLC?
      • Fonts and Graphics on Tools broken after Interact Upgrade to Ver 7 to run on PA2 hardware. Application runs but FONT Size or images are wrong.
      • GESNP / GESNPX 9030 / 9070 Serial Com configuration for Interact / PowerStation PA/PA2/P13 etc...
      • I need more fonts for my Interact application.
      • INTERACT How to Order
      • Interact screen size too BIG or too small after upgrade. Only see part of screen or screen compressed in top left corner of display.
      • Legacy Product Page - P1 Series
      • Legacy Product Page - P2 Series
      • Legacy Product Page - P3, P4, P5 and P7 Series
      • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
      • Security Key not found or Not programmed to support Module or Driver
      • Which HMI runs Interact?
    • InteractX+
    • Interact Xpress+
    • IXA / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (Discontinued)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • PFD - Parker Factory Display (Discontinued)+
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Legacy Product Page - P1 Series

Print Friendly and PDF

Introduction

The P1 series was a line of DOS-based HMIs running Parker CTC's Interact runtime software. There were many variants of the P1, the only one of which still available is the P13.

Models

The following models are covered under this series:

  • P11-*
  • P12-*
  • P15-*
  • P1H-*
  • PMP-*

Replacement Options

For most P1 models (P11, P12, PMP, P1H), the best replacement is the P13 [ Product Page ]. For the P15, the best option is the PA210 [ Product Page ]. There are a few exceptions to this:

  • Units with PC/104 cards installed (e.g. Allen-Bradley Blue Hose communications card).
  • Units running custom software beyond the Interact runtime. Occasionally, certain machine builders would install additional software on the P21 and use it to do things outside Interact's capabilities. This is very rare.
  • Applications that use a printer. Printers are no longer supported.

We recommend talking with Parker or your distributor before attempting an upgrade.

Related Articles

  • How do I transfer my old Interact application to a newer Interact panel?

Documentation

Model Number Manual Title Manual Part Number Revision Date File Size
P11-TOUCH P1 Touchscreen A3-04983-100 4/97 111KB
BLR-6050 P1 Backlight Bulb A3-04986-100 4/97 226KB
P11-X1XDR-3 P1 User Guide A3-05087-101 4/98 1.0M
A3-05087-102 3/99 1.0M
A3-05087-105 11/99 1.1M
P1X-2000 P1 Compact Flash Installation Replacement A3-05565-100 10/99 10KB
P1X-PC104 P1P PC/104 Installation Guide A3-05741-100 5/99 66KB
A3-05741-101 2/01 56KB
P11-X1XDR-3 P1 Release Notes A3-06029-100 2/00 5KB
PMP-X1XDM MotionPanel QuickStart Guide A3-06165-101 9/00 141KB
A3-06165-102 3/03 127KB
PMP-X1XDM MotionPanel User Guide A3-06166-100 9/00 970KB
A3-06166-101 3/03 691KB
P12-X44DR P1 Pentium User Guide A3-06170-100 1/01 883KB
P1H-X14DR P1H Instruction Sheet A3-06190-100 10/00 5KB
MOD-5160-H/PP1-5161-K P1H Upgrade Instructions A3-06191-100 2/01 111KB
A3-06191-101 4/03 91KB
P12-X44DR P1 P Touchscreen Install. Guide A3-06205-100 2/01 235KB
DSP-1004 Display Replacement A3-06240-100 2/01 78KB
A3-06240-101 7/02 85KB
N/A P1 10" User Guide A3-06509-100 4/02 473KB
BLR-6051 P1P STN Backlight Replacement A3-06547-100 7/02 68KB
N/A P1-10" PowerStation Release Note A3-06609-100 3/03 16KB

09JUL2021 DCLIFFE

  • p12
  • INTERACT
  • p1h
  • P11
  • CTC
  • P1
  • pmp
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply