Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Legacy Product Page - P2 Series
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Legacy Product Page - P2 Series
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
  • Visualization and Human Machine Interface (HMI)-
    • Interact (Legacy)-
      • Replace/Upgrade Interact panel P11/P1H/P15/P2/P3/P4/P5 etc
      • CTC and i-Motors
      • Configure a TCP/IP Dial-Up Adapter Connection.
      • Interact Misc - Can ASCII register in the PLC be used as an alarm?
      • Configure a TCP/IP connection (IP address)
      • Compact Flash Disk Transfer using Interact MachineShop Toolbar to Upload and Download
      • ERROR - Invalid Panel list or Key Pad Address.
      • Ethernet download to a CTC Panel.
      • How to Restore Motion Panel.
      • Interact Software - Display alarms in a RMD tool within PTM
      • How to run app on my PowerStation on boot-up?
      • Implementing the New CMOT Driver
      • LEDs on the back of the Profibus card
      • MachineLogic - How do I clear Retentive Memory?
      • MachineLogic - No project on the PLC.
      • Security Key Setup not Installed
      • Single layer SST 5136-PFB-104 card with Interact.
      • TCP/IP Ethernet and a Dial-Up Connection
      • TCP/IP open port failure
      • Can I run Interact 6.X in Windows NT/2K/XP?
      • Can I run Interact7 on my Windows 10 or 7 PC?
      • Configure a TCP/IP connection (DHCP)
      • Configure a TCP/IP direct Ethernet connection
      • CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Enable/disable the screen saver
      • Flashback Utilities for the CTC DOS Based PowerStations - If you have Interact ver 7 it installs all the necessary Flashbacks.
      • HMI Battery Replacements
      • How do I connect my P13, PA or PA2 Interact HMI to DataHighway Plus Network?
      • How do I recalibrate my Interact touchscreen? Or change the panel's ethernet address?
      • How do I show hidden and protected files in Windows?
      • How do I transfer my old Interact application to a newer Interact panel?
      • How to connect my device to Interact? Interact Cable Dictionary
      • How to print graphics from Interact run mode.
      • I upgraded my old hardware to a PA2 and have Vertical Stripes on screen and does not load my application.
      • Interact does not recognize the security key.
      • Interact: Error Initializing AMM - Invalid Logging Path
      • Minimum of NT 4.0 SP3 to install Machine Shop
      • Powerstation Shell on older CTC units
      • Replacing old HMIs that run Interact
      • Upgrading from a PA to a PA2
      • What are Interact Runtime modules?
      • Whats the difference between FLH-0512P and FLH-0512?
      • What internal variable can I use to R/W ASCII?
      • Interact Troubleshooting - WinXP- cannot select options on Toolbar
      • Control Access to Panels and Tools using the Password User Levels in Interact
      • Driver for my Allen Bradley Micrologix 1500 PLC?
      • Fonts and Graphics on Tools broken after Interact Upgrade to Ver 7 to run on PA2 hardware. Application runs but FONT Size or images are wrong.
      • GESNP / GESNPX 9030 / 9070 Serial Com configuration for Interact / PowerStation PA/PA2/P13 etc...
      • I need more fonts for my Interact application.
      • INTERACT How to Order
      • Interact screen size too BIG or too small after upgrade. Only see part of screen or screen compressed in top left corner of display.
      • Legacy Product Page - P1 Series
      • Legacy Product Page - P2 Series
      • Legacy Product Page - P3, P4, P5 and P7 Series
      • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
      • Security Key not found or Not programmed to support Module or Driver
      • Which HMI runs Interact?
    • InteractX+
    • Interact Xpress+
    • IXA / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (Discontinued)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • PFD - Parker Factory Display (Discontinued)+
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Legacy Product Page - P2 Series

Print Friendly and PDF

Introduction

The P2 series (also known as the P21 series) was a line of DOS-based HMIs running Parker CTC's Interact runtime software.

Models

This series covered all models with model number format P21-*. Most P21 model numbers followed the format given in the below catalog sample. This sample does not show every option ever offered, but is a good reference for understanding what options were installed on a unit.

Older models had a format in the style P21-012DR. The important thing to note is that models in this vintage may have been shipped with SIMM stick memory instead of Compact Flash, making it more difficult to recover programs from them when they fail.

Replacement Options

Most P21s can be replaced by the PA210 [ Product Page ]. There are a number of exceptions to this:

  • Units with PC/104 or ISA cards installed (e.g. Allen-Bradley Blue Hose communications card).
  • Units running custom software beyond the Interact runtime. Occasionally, certain machine builders would install additional software on the P21 and use it to do things outside Interact's capabilities. This is very rare.
  • Applications that use a printer. Printers are no longer supported.

We recommend talking with Parker or your local distributor before attempting an upgrade.

Related Articles

  • How do I transfer my old Interact application to a newer Interact panel?

Documentation

Model Number Manual Title Manual Part Number Revision Date File Size
P21-XXX-AX-1DX P2 User Guide A3-05425-100 3/98 611KB
A3-05425-101 2/99 1MB
A3-05425-105 11/99 931KB
A3-05425-106 10/00 895KB
P2X-PC104 P2 PC/104 Installation A3-05434-100 3/98 81KB
A3-05434-101 10/00 81KB
P21-XXX-AX-1DX P2 Touchscreen Serial Driver Installation A3-05662-100 3/99 14KB
DIM-OXXX P2-P5 Pentium PowerStation DRAM Replacement A3-06111-100 10/00 666KB
N/A P2 5x86 Calibration Guide A3-06209-100 11/00 25KB
P21-XXX-AX-1DX P2 5x86 CPU Manual PCA6145 01/97 431KB

12JUL2021 DCLIFFE

  • INTERACT
  • CTC
  • P2
  • P21
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply