Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Legacy Product Page - P3, P4, P5 and P7 Series
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Legacy Product Page - P3, P4, P5 and P7 Series
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
  • Visualization and Human Machine Interface (HMI)-
    • Interact (Legacy)-
      • Replace/Upgrade Interact panel P11/P1H/P15/P2/P3/P4/P5 etc
      • CTC and i-Motors
      • Configure a TCP/IP Dial-Up Adapter Connection.
      • Interact Misc - Can ASCII register in the PLC be used as an alarm?
      • Configure a TCP/IP connection (IP address)
      • Compact Flash Disk Transfer using Interact MachineShop Toolbar to Upload and Download
      • ERROR - Invalid Panel list or Key Pad Address.
      • Ethernet download to a CTC Panel.
      • How to Restore Motion Panel.
      • Interact Software - Display alarms in a RMD tool within PTM
      • How to run app on my PowerStation on boot-up?
      • Implementing the New CMOT Driver
      • LEDs on the back of the Profibus card
      • MachineLogic - How do I clear Retentive Memory?
      • MachineLogic - No project on the PLC.
      • Security Key Setup not Installed
      • Single layer SST 5136-PFB-104 card with Interact.
      • TCP/IP Ethernet and a Dial-Up Connection
      • TCP/IP open port failure
      • Can I run Interact 6.X in Windows NT/2K/XP?
      • Can I run Interact7 on my Windows 10 or 7 PC?
      • Configure a TCP/IP connection (DHCP)
      • Configure a TCP/IP direct Ethernet connection
      • CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Enable/disable the screen saver
      • Flashback Utilities for the CTC DOS Based PowerStations - If you have Interact ver 7 it installs all the necessary Flashbacks.
      • HMI Battery Replacements
      • How do I connect my P13, PA or PA2 Interact HMI to DataHighway Plus Network?
      • How do I recalibrate my Interact touchscreen? Or change the panel's ethernet address?
      • How do I show hidden and protected files in Windows?
      • How do I transfer my old Interact application to a newer Interact panel?
      • How to connect my device to Interact? Interact Cable Dictionary
      • How to print graphics from Interact run mode.
      • I upgraded my old hardware to a PA2 and have Vertical Stripes on screen and does not load my application.
      • Interact does not recognize the security key.
      • Interact: Error Initializing AMM - Invalid Logging Path
      • Minimum of NT 4.0 SP3 to install Machine Shop
      • Powerstation Shell on older CTC units
      • Replacing old HMIs that run Interact
      • Upgrading from a PA to a PA2
      • What are Interact Runtime modules?
      • Whats the difference between FLH-0512P and FLH-0512?
      • What internal variable can I use to R/W ASCII?
      • Interact Troubleshooting - WinXP- cannot select options on Toolbar
      • Control Access to Panels and Tools using the Password User Levels in Interact
      • Driver for my Allen Bradley Micrologix 1500 PLC?
      • Fonts and Graphics on Tools broken after Interact Upgrade to Ver 7 to run on PA2 hardware. Application runs but FONT Size or images are wrong.
      • GESNP / GESNPX 9030 / 9070 Serial Com configuration for Interact / PowerStation PA/PA2/P13 etc...
      • I need more fonts for my Interact application.
      • INTERACT How to Order
      • Interact screen size too BIG or too small after upgrade. Only see part of screen or screen compressed in top left corner of display.
      • Legacy Product Page - P1 Series
      • Legacy Product Page - P2 Series
      • Legacy Product Page - P3, P4, P5 and P7 Series
      • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
      • Security Key not found or Not programmed to support Module or Driver
      • Which HMI runs Interact?
    • InteractX+
    • Interact Xpress+
    • IXA / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (Discontinued)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • PFD - Parker Factory Display (Discontinued)+
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Legacy Product Page - P3, P4, P5 and P7 Series

Print Friendly and PDF

Introduction

The P3, P4, P5 and P7 series were lines of DOS-based HMIs running Parker's Interact runtime software. While they all had similar software and a similar hardware architecture, each series had a few differentiating features. A summary of each series, taken from old PowerStation literature, is shown below.

Models

These series covered all models with model number format P31-*, P41-*, P50-*, P51-* and P71-*. Model number formats are given in the below catalog samples. These samples do not show every option ever offered, but are good references for understanding what options were installed on a unit.

Older models had a format in the style P50-21AR-A. The important thing to note is that models in this vintage may have been shipped with SIMM stick memory instead of Compact Flash, making it more difficult to recover programs from them when they fail.

Replacement Options

Many of these models can be replaced by the PA2 [ Product Page ]. There are a number of exceptions to this:

  • The P5 had a full set of physical function keys and a larger cutout. Parker no longer offers an Interact HMI with function keys. However, it may still be possible to migrate to a PA2 since function keys on the P5 were typically "mirrors" for existing touchable buttons in the Interact runtime. Contact Parker for assistance.
  • Units with PC/104 or ISA cards installed (e.g. Allen-Bradley Blue Hose communications card).
  • Units running custom software beyond the Interact runtime. Occasionally, certain machine builders would install additional software on the P21 and use it to do things outside Interact's capabilities. This is very rare.
  • Applications that use a printer. Printers are no longer supported.

We recommend talking with Parker or your local distributor before attempting an upgrade.

Related Articles

  • How do I transfer my old Interact application to a newer Interact panel?

Documentation

Model Number Manual Title Manual Part Number Revision Date File Size
COV-4000 PowerStation Card Extension Cover A3-04934-102 4/98 138KB
A3-04934-103 10/98 250KB
BLR-6080 TFT Backlight Bulb Replacement A3-05183-100 4/98 32KB
A3-05183-105 9/99 90KB
P31-XCX-XX-2AX, P41-XXX-XX-2XX, P5X-XXX-XX-2XX, P7X-XXX-XX-2XX (version 105 only) PowerStation User Guide A3-05190-101 4/98 707KB
A3-05190-102 10/98 1.2MB
A3-05190-105 10/99 1.2MB
A3-05190-106 8/00 1.3MB
BLR-6090 LCD Backlight Bulb Replacement A3-05192-100 4/98 63KB
A3-05192-105 9/99 154KB
BLR-6060 STN Backlight Bulb Replacement A3-05193-101 3/98 86KB
A3-05193-105 9/99 246KB
RAM-40XX PowerStation DRAM Replacement A3-05196-101 4/98 85KB
A3-05196-102 10/98 55KB
P31-XCX-XX-2AX, P41-XXX-XX-2XX, P5X-XXX-XX-2XX PowerStation Contrast/Brightness Utility A3-05211-100 4/98 10KB
A3-05211-101 10/98 9KB
A3-05211-105 11/99 13KB
PCON-232-A, PCON-422-A, PCON-485-A 5x86 Third Serial Port Installation A3-05665-100 2/99 977KB
A3-05665-105 11/99 946KB
DIM-OXXX P2-P5 Pentium PowerStation DRAM Replacement A3-06111-100 10/00 666KB
PCOM-232(A), PCOM-422(A), PCOM-485(A) Pentium Third Serial Port A3-06229-100 2/01 904KB

05AUG2021 DCLIFFE

  • P7
  • P3
  • INTERACT
  • CTC
  • P41
  • P50
  • P71
  • P4
  • P51
  • P31
  • P5
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply