ACR9000 ModuFlex
Pin5-------------Pin1 (CAN_SHLD)
Pin3-------------Pin3 (CAN_GND)
Pin7-------------Pin4 (CAN_H)
Pin2-------------Pin5 (CAN_L)
Pin2 (CAN_V+) on the ModuFlex must be supplied from an
external 24Vdc power supply. Pin9 on the ACR9000,
labeled CAN_V+, is not to be connected to the CAN_V+
terminal of the ModuFlex.