Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base INTERACT How to Order
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base INTERACT How to Order
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
  • Visualization and Human Machine Interface (HMI)-
    • Interact (Legacy)-
      • Replace/Upgrade Interact panel P11/P1H/P15/P2/P3/P4/P5 etc
      • CTC and i-Motors
      • Configure a TCP/IP Dial-Up Adapter Connection.
      • Interact Misc - Can ASCII register in the PLC be used as an alarm?
      • Configure a TCP/IP connection (IP address)
      • Compact Flash Disk Transfer using Interact MachineShop Toolbar to Upload and Download
      • ERROR - Invalid Panel list or Key Pad Address.
      • Ethernet download to a CTC Panel.
      • How to Restore Motion Panel.
      • Interact Software - Display alarms in a RMD tool within PTM
      • How to run app on my PowerStation on boot-up?
      • Implementing the New CMOT Driver
      • LEDs on the back of the Profibus card
      • MachineLogic - How do I clear Retentive Memory?
      • MachineLogic - No project on the PLC.
      • Security Key Setup not Installed
      • Single layer SST 5136-PFB-104 card with Interact.
      • TCP/IP Ethernet and a Dial-Up Connection
      • TCP/IP open port failure
      • Can I run Interact 6.X in Windows NT/2K/XP?
      • Can I run Interact7 on my Windows 10 or 7 PC?
      • Configure a TCP/IP connection (DHCP)
      • Configure a TCP/IP direct Ethernet connection
      • CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Enable/disable the screen saver
      • Flashback Utilities for the CTC DOS Based PowerStations - If you have Interact ver 7 it installs all the necessary Flashbacks.
      • HMI Battery Replacements
      • How do I connect my P13, PA or PA2 Interact HMI to DataHighway Plus Network?
      • How do I recalibrate my Interact touchscreen? Or change the panel's ethernet address?
      • How do I show hidden and protected files in Windows?
      • How do I transfer my old Interact application to a newer Interact panel?
      • How to connect my device to Interact? Interact Cable Dictionary
      • How to print graphics from Interact run mode.
      • I upgraded my old hardware to a PA2 and have Vertical Stripes on screen and does not load my application.
      • Interact does not recognize the security key.
      • Interact: Error Initializing AMM - Invalid Logging Path
      • Minimum of NT 4.0 SP3 to install Machine Shop
      • Powerstation Shell on older CTC units
      • Replacing old HMIs that run Interact
      • Upgrading from a PA to a PA2
      • What are Interact Runtime modules?
      • Whats the difference between FLH-0512P and FLH-0512?
      • What internal variable can I use to R/W ASCII?
      • Interact Troubleshooting - WinXP- cannot select options on Toolbar
      • Control Access to Panels and Tools using the Password User Levels in Interact
      • Driver for my Allen Bradley Micrologix 1500 PLC?
      • Fonts and Graphics on Tools broken after Interact Upgrade to Ver 7 to run on PA2 hardware. Application runs but FONT Size or images are wrong.
      • GESNP / GESNPX 9030 / 9070 Serial Com configuration for Interact / PowerStation PA/PA2/P13 etc...
      • I need more fonts for my Interact application.
      • INTERACT How to Order
      • Interact screen size too BIG or too small after upgrade. Only see part of screen or screen compressed in top left corner of display.
      • Legacy Product Page - P1 Series
      • Legacy Product Page - P2 Series
      • Legacy Product Page - P3, P4, P5 and P7 Series
      • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
      • Security Key not found or Not programmed to support Module or Driver
      • Which HMI runs Interact?
    • InteractX+
    • Interact Xpress+
    • IXA / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (Discontinued)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • PFD - Parker Factory Display (Discontinued)+
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
INTERACT How to Order

Print Friendly and PDF

Interact

  • PA2 and P13 units are pre-loaded with Interact7 runtime.
  • ALL optional runtime modules are included with every PA2 and the P13. 
  • Interact Software is only compatible with Windows XP and will not work in Window 7 XP Mode, or newer versions of Windows (Win8, Win8.1 or Win10).
  • If users have any version of Interact 6 or 5, Interact Software upgrade is REQUIRED. The upgrade part numbers can be used to purchase upgrades.
  • For users that do not have Interact, MSP-7NA0-P is the part number to purchase.

Contact your local Parker Automation Technology Center (ATC) distributor for purchasing.

Interact 7 Development software Part numbers:  

Model # Description
MSP-7NA0-P    Interact7 Development (new user)
IUP-6070-6 Interact Development Upgrade to 7.X from 6.X
IUP-6070-5 Interact Development Upgrade to 7.X from 5.X

 

Runtime and Development softwares

Runtime software is the software the HMI is running. HMIs are touchscreen computers allowing machine operators to start/stop machines, select different parts or recipes to run, input different parameters or monitor the machine status. In general Interact panels are can be thought of as a touchscreen computer version of a machine control panel. HMIs can communicate to different PLCs or motion controllers via different those devices different communication protocols. Newer HMIs can be used for interfacing to computer servers (InteractX) or monitor other HMIs (InteractX) or machines or provide remote access (Xpress or InteractX).  Parker HMIs include a runtime license installed. Each HMI requires a runtime license.

Development software is the software machine builders and programmers use to develop or update the HMI projects that are downloaded to the HMIs that run in the runtime software. Projects can be transferred to the HMI via Compact Flash cards or directly via ethernet or serial communications. Projects can be setup with different levels of users to prevent access to parts of the projects (machine operators, engineers, admin). The development software is purchased once and can be used to develop the project.

 

PA2 and P13

PA2 and P13 require projects developed in Interact version 7.0 software. Interact software to develop new projects or upgrade projects from older PowerStations. Interact software is an additional purchase. Interact software can be used to upgrade or develop multiple HMI projects.  PA2s and P13s can run projects developed in older versions of Interact, but must first be upgraded using Interact 7. Note there are differences in the hardware for PowerStations. PA2s and P13s do not have PC104 or ISA expansion slots and only have 2 serial ports. Applications using PC104 or ISA expansion slots or 3 serial ports would need updating.

  

Older PowerStations (PA, PS10, etc)

Interact 7.0 can be used to modify projects for older PowerStations. Older versions of Interact are no longer available nor supported. Version 7.0 can be used and is not checking the HMI for hardware licenses for the modules and includes all modules that could be used in a project.  With older versions of PowerStations like the PA, runtime modules were selected with additional cost to the hardware.

 

CompactFlash Cards and Spare Parts

Part Number Description
FLH-0512P Spare Compact Flash (CF) card for Interact HMIs (PA2, P13 or PA)

PA2 and P1 PowerStations include a compact flashcard, power connector and mounting clips. For spares, FLH-0512P is the part number for the 512MB compact flash card for the CTC legacy products, or any unit running INTERACT. (This includes PA/P13/PA2). This is a bootable CF card.  Contact your local Parker Automation Technology Center (ATC) distributor for purchasing.

 

Kits include mounting clips and power connectors:

Part Number Description
KIT-1500 10" PA/P1/PS/EPX/HPX/PX/HPC/PC/IPX/IPC/XPR/XPC/PA2/PHM/PM1     
KIT-1600 5"/6"/8" PA/EPX08, XPC06 or XPC08, XPR06 or XPR08, PA206 or PA208
KIT-9000 12" PS/PX/PC/Monitors
KIT-9000 15" PA/PS/EPX/HPX/PX/HPC/PC/IPX/IPC/XPR/XPC/PA2/PHM/PM1

Related FAQ:  CTC/HMI: Connector Part Numbers

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply