Users and repair facilities can purchase parts for the SSD Drives.
Most parts are listed in the user manual.
However, some parts may have numbers on them in addition to the model number to use for ordering.
AH469910U001 This is the PCB number on a control card for an 890.
It's sold under 8904 part numbers. Same card is used in 2 different versions, one standard, the second is conformally coated. Select as appropriate:
Pricing and delivery available through distributors, on our distributor extranet tool.
4/22jh