Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How does the password protection feature work in the AC10 (via the keypad)?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How does the password protection feature work in the AC10 (via the keypad)?
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
  • AC/DC Industrial Drives-
    • AC10-
      • AC10 Heat Dissipation
      • AC10: Is the keypad detachable during operation?
      • AC10: Why am I getting over-voltage trips?
      • AC10: Why is my AC motor running hot?
      • Can I program through the keypad and DSELite on the AC10?
      • How can I configure an AC10 to run at two different speeds without using an analog input?
      • How do I connect an AC10 to a TS8000?
      • How do I clone the AC10 with the 1002-00 module?
      • How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and PDB?
      • How do I implement a Fast Stop circuit on the AC10?
      • How do I know what firmware revision my AC10 is?
      • How do I reset an AC10 back to factory defaults?
      • How do I reset the master password in an AC10?
      • How do I set up an AC10 for torque control?
      • In what type of package is the AC10 available?
      • What are the basic parameters to run an AC Induction motor from just the keypad?
      • What are the basic wiring connections of the AC10?
      • What are the environmental operating conditions for the AC10?
      • What are the minimum and maximum 3-phase input voltage ratings for the AC10?
      • What default configurations are available for the AC10?
      • What is the current overload rating for the AC10 drive?
      • What kind of I/O is available on the AC10?
      • What safety standards does the AC10 meet?
      • What software and communication cable are used for programming an AC10?
      • Why won't my AC10 run my motor?
      • AC10 Modbus-RTU Example to Interact Xpress HMI (XTA)
      • Can an AC10 run a PMAC motor?
      • How does the password protection feature work in the AC10 (via DSE Lite)?
      • How does the password protection feature work in the AC10 (via the keypad)?
      • Updated Control Terminal Torque Specifications for AC10 VFD’s
      • When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.
      • Where do I get the AC10's Modbus RTU / programming connector?
    • AC30+
    • DC590+ Series+
    • AC890 Series+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • AC15/AC20
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
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
How does the password protection feature work in the AC10 (via the keypad)?

Print Friendly and PDF

Password protection in the AC10 prevents the majority of the parameters from being changed.  Many parameters values can still be viewed via the keypad though.

If the keypad shows alarm code Err1 when you attempt to change a parameter then password protection is currently enabled on that drive.

This password protection will also prevent cloning the drive's current parameter settings or loading parameters from a cloning device.  Neither of these operations will be possible until the current password has been entered in the F100 parameter at a minimum.  If attempted on a password protected drive you will see alarm code Er73 on the display.

F107 is used to enable/disable the password feature.  F107=1 enables password protection.

F108 is used to set the user password (which has a range of 0 -> 9999).  (default value of F108 = 8)

F100 is used to enter the password if the feature (F107=1) has been enabled.

   


 

To set up initially

1.  Change F108 to the desired password value (0 through 9999).

2.  Change F107 to a value of 1.

Password protection is now enabled.  Any further changes will require you to enter the set password value into parameter F100 before you can make changes.

Note - Once password protection is enabled, F108 will not display what the password is currently set to nor will you be able to reset to factory default via the F160=1 parameter setting so use caution and make sure you know what you have set F108 value to BEFORE you set F107 to a value of 1.  There is not a secret 'backdoor'.

  


 

To change password (or disable the feature)

1.  Set F100 to the currently configured password value (0 through 9999).

This has now temporarily disabled the password protection (until a power cycle or F107 is set to 1 again manually).

2.  Change F108 to whatever new password value you want to use (0 through 9999).

3.  To disable the password feature going forward, now change F107 value to 0.  

 

   

 Related FAQ

How does the password protection feature work in the AC10 (via DSE Lite)?

 

 

 


glh   May 2022

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply