Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How does the password protection feature work in the AC10 (via DSE Lite)?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How does the password protection feature work in the AC10 (via DSE Lite)?
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
  • AC/DC Industrial Drives-
    • AC10-
      • AC10 Heat Dissipation
      • AC10: Is the keypad detachable during operation?
      • AC10: Why am I getting over-voltage trips?
      • AC10: Why is my AC motor running hot?
      • Can I program through the keypad and DSELite on the AC10?
      • How can I configure an AC10 to run at two different speeds without using an analog input?
      • How do I connect an AC10 to a TS8000?
      • How do I clone the AC10 with the 1002-00 module?
      • How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and PDB?
      • How do I implement a Fast Stop circuit on the AC10?
      • How do I know what firmware revision my AC10 is?
      • How do I reset an AC10 back to factory defaults?
      • How do I reset the master password in an AC10?
      • How do I set up an AC10 for torque control?
      • In what type of package is the AC10 available?
      • What are the basic parameters to run an AC Induction motor from just the keypad?
      • What are the basic wiring connections of the AC10?
      • What are the environmental operating conditions for the AC10?
      • What are the minimum and maximum 3-phase input voltage ratings for the AC10?
      • What default configurations are available for the AC10?
      • What is the current overload rating for the AC10 drive?
      • What kind of I/O is available on the AC10?
      • What safety standards does the AC10 meet?
      • What software and communication cable are used for programming an AC10?
      • Why won't my AC10 run my motor?
      • AC10 Modbus-RTU Example to Interact Xpress HMI (XTA)
      • Can an AC10 run a PMAC motor?
      • How does the password protection feature work in the AC10 (via DSE Lite)?
      • How does the password protection feature work in the AC10 (via the keypad)?
      • Updated Control Terminal Torque Specifications for AC10 VFD’s
      • When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.
      • Where do I get the AC10's Modbus RTU / programming connector?
    • AC30+
    • DC590+ Series+
    • AC890 Series+
    • AC15/AC20+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
    • Constant Torque (CT) versus Variable Torque (VT) in VFDs
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
How does the password protection feature work in the AC10 (via DSE Lite)?

Print Friendly and PDF

To enable the password protection feature in an AC10 via your DSE Lite download, find the Password block and double click on it to change its values.

You can change the password value itself (supports values from 0 to 9999 for the password value) and then change the ENABLE input to TRUE.  You can then do an Install or Full Install to send this down to the drive and once complete, the password will be set to your value and enabled. 

DO NOT use the Full Install option unless you have previously extracted the particular drive's existing parameters into your template for your starting point, since a full install will also change and overwrite all of the 'pink' values showing in the DSE Lite template.  This includes basic motor data as well as some underlying drive frame size specific data.  If you do a Full Install and your template doesn't contain the correct "Frame Dependent" values you may corrupt your drive's configuration and render it inoperable.

Note - Once password protection is enabled, F108 will not display what the password is currently set to nor will you be able to reset to factory default via the F160=1 parameter setting so use caution and make sure you know what you are setting the password value to BEFORE you initial the install procedure.  There is not a secret 'backdoor'.

 


To determine if the drive has the password feature enabled (factory default is disabled and F108 value is 8 by default), you can do a Refresh Full from the Command menu.  You will see this reference in the Scratch Pad.

 

When the drive is in password protection mode, you can still go online to monitor parameters.  However, you will not be able to Extract the parameters.  Trying to extract parameters will result in this error.  Nor will parameter F108 report the actual password value currently set, it will only show 0 in this case.

To allow subsequent installs (Install or Full Install) or parameter extraction (Extract Drive Parameters), you will need to enter the current password value via parameter F100 on the keypad.  Once temporarily unlocked, you can extract or install as needed.  Once an install has completed, the drive will automatically be reset and thus the password will be re-enabled unless your configuration download set the F107 parameter back to FALSE.

  

  

Another related FAQ:

How does the password protection feature work in the AC10 (via the keypad)?

 

 

 

 

glh  5/2022

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply