Go to Parker.com
  • Sign in
Technologies
  • Aerospace
  • Climate Control
  • Electromechanical Group
  • Filtration
  • Fluid and Gas Handling
  • Hydraulics
  • IoT
  • Pneumatics
  • Process Control
  • Sealing and Shielding
Other Groups
  • Parker Indego
Blogs Forums Knowledge Bases
Parker Community
Parker Community
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
    Other Groups
    • Parker Indego
    Blogs Forums Knowledge Bases
  • User
  • Site
  • Search
  • User
Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.
  • Electromechanical – Industrial Support Forum
  • Electromechanical Industrial Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical - Industrial requires membership for participation - click to join
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives-
    • AC10-
      • AC10 Heat Dissipation
      • AC10: Is the keypad detachable during operation?
      • AC10: Why am I getting over-voltage trips?
      • AC10: Why is my AC motor running hot?
      • Can I program through the keypad and DSELite on the AC10?
      • How can I configure an AC10 to run at two different speeds without using an analog input?
      • How do I connect an AC10 to a TS8000?
      • How do I clone the AC10 with the 1002-00 module?
      • How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and PDB?
      • How do I implement a Fast Stop circuit on the AC10?
      • How do I know what firmware revision my AC10 is?
      • How do I reset an AC10 back to factory defaults?
      • How do I reset the master password in an AC10?
      • How do I set up an AC10 for torque control?
      • In what type of package is the AC10 available?
      • What are the basic parameters to run an AC Induction motor from just the keypad?
      • What are the basic wiring connections of the AC10?
      • What are the environmental operating conditions for the AC10?
      • What are the minimum and maximum 3-phase input voltage ratings for the AC10?
      • What default configurations are available for the AC10?
      • What is the current overload rating for the AC10 drive?
      • What kind of I/O is available on the AC10?
      • What safety standards does the AC10 meet?
      • What software and communication cable are used for programming an AC10?
      • Why won't my AC10 run my motor?
      • AC10 Modbus-RTU Example to Interact Xpress HMI (XTA)
      • Can an AC10 run a PMAC motor?
      • How does the password protection feature work in the AC10 (via DSE Lite)?
      • How does the password protection feature work in the AC10 (via the keypad)?
      • Updated Control Terminal Torque Specifications for AC10 VFD’s
      • When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.
      • Where do I get the AC10's Modbus RTU / programming connector?
    • AC30+
    • DC590+ Series+
    • AC890 Series+
    • AC15/AC20
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
  • Servo Motors+
  • Step Motors+
  • Linear and Rotary Positioners+
  • Electric Cylinders+
  • T-Slot Aluminum Framing+
  • C3 + Xpress + ETH+
  • How can I stay updated on Parker electromechanical and drives product news?
  • Legacy (Discontinued)+
  • Other+
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
Wiki Actions
  • Share
  • More
  • Cancel
Community Quick Links
  • Home
  • Technologies
    • Aerospace
      • Supplier Resource Center
    • Climate Control
    • Electromechanical Group
      • Electromechanical - Industrial
      • Electromechanical – Mobile
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
      • Pneumatic Industrial
      • Pneumatics Mobile
    • Process Control
    • Sealing and Shielding
  • Other Groups
    • Parker Indego
      • Parker Indego Instructors
      • Parker Indego Therapists
      • Parker Indego Distributors
  • Community Blogs
  • Community Forums
  • Community Knowledge Bases
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.

Print Friendly and PDF

You try to do an Install or Full Install from DSE Lite to your AC10 and nothing seems to happen.

 

First, try doing a Refresh Full from the Command menu and observe the response in the Scratch Pad.  The response should note the AC10 firmware revision, power level and voltage, and that you are actually connected via DSE Lite).  If you do not see this then you have more fundamental communications problems.  Verify your cable connection and/or USB converter if using one.

 

If you are connected, and observe this symptom, then the most likely cause of this is that the drive is currently in RUN mode.  Check the LED indicators on the keypad and see if the RUN led is lit.

Use the red "O" button to take the drive out of RUN mode and then you should be able to do your configuration Install or Full Install.

Unfortunately, there is not an indication in DSE Lite that the drive is still in RUN mode. 

 
Note - a Full Install should only be done if you have first done a Parameter Extraction into your template (or your saved configuration file is for this particular drive and frame size) as a starting point as a Full Install will also overwrite some Frame Dependent parameters and if these are changed to something different than what your drive is, the drive may be rendered inoperable.

 

 

 

 


glh  5/2022

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Related
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

Parker Hannifin Parker Hannifin

  • Products
  • About Parker
  • Investors
  • Community
  • Careers

Global Operations Global Operations

  • Divisions
  • Sales Companies
  • Worldwide Locations
  • Distribution Network
  • ParkerStore™ Network

Company Information Company Information

  • Newsroom
  • Event Calendar
  • Working with Parker
  • Product Brands
  • History

Global Support Center Global Support Center

  • Support
  • CAD
  • Where to Buy
  • Contact Parker
  • Manage Online Orders
© Parker Hannifin Corp 2023
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.