Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base 6053 DNET Techbox Firmware Incompatibilities
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base 6053 DNET Techbox Firmware Incompatibilities
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
  • AC/DC Industrial Drives-
    • AC10+
    • AC30+
    • DC590+ Series+
    • AC890 Series+
    • AC15/AC20+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
    • Constant Torque (CT) versus Variable Torque (VT) in VFDs
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
6053 DNET Techbox Firmware Incompatibilities

Print Friendly and PDF

A system commissioned with a Eurotherm DeviceNet techbox will not work if it is replaced with an SSD DeviceNet product.This will affect customers who ordered their drive product / system after 13th March 2006.

This is a legacy issue, and the DNET techboxes were suddenly discontinued in September 2022.

There is no firmware available from Parker Hannifin for these techboxes to upgrade/downgrade them, there is no upgrade/downgrade procedure. This was a Devicenet issue regarding vendor identification schemes.

  • Here's the discontinuance bulletin

  • See this Appnote

Summarizing:
The DeviceNet standard, issued by the ODVA (Open DeviceNet Vendors Association) requires all DeviceNet products to incorporate a Vendor Identifier (a unique number allocated by them to each manufacturer of DeviceNet products).
When SSD departed from Eurotherm, there was a requirement to remove Eurotherm from all documentation including the DeviceNet Vendor Identifier. This change was effected in V4.1 Firmware for the DeviceNet product (can be identified from drive keypad).

Customers who are replacing old 6053 / 6055 DeviceNet Techboxes with new one will experience a communication conflict that will stop the operation of the DeviceNet within the installed system. 

Customers may experience an intermittent dropping out of DNET cards as well. This can in many cases be triggered by, or look like, electrical noise on the system causing the communications to drop out. If the DNET option cards look as if they are supposed to function with the LEDs indiciating good health status, but a power cycle rectifies the issue (it does not automatically reconnect) then the issue likely stems from the incompatibilities that comes with the v4.1firmware on the cards.

JD 16NOV22

  • compatibile
  • 6053
  • firmware
  • DNET
  • incompatibile
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply