Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base DESAT (OVER I) Fault
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base DESAT (OVER I) Fault
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
  • AC/DC Industrial Drives-
    • AC10+
    • AC30+
    • DC590+ Series+
    • AC890 Series+
    • AC15/AC20+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
    • Constant Torque (CT) versus Variable Torque (VT) in VFDs
    • DSE890 and DSELite Ethernet Connection Port Numbers
    • ACxx scope tool problems with Windows 11
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
DESAT (OVER I) Fault

Print Friendly and PDF

DSAT (OVER I) frequently means something shorted on the output. The manual in product will point to 'overcurrent' for additinal sanity checks. After going through 'Overcurrent' for the respective product, see below:

  • Try taking the motor leads loose and running the drive in V/Hz mode. If it still trips, there is a problem on the IGBT bridge.
  • If it does not trip, then it is likely one of the following is true:
    • There is a short in the motor (phase to phase, or phase to ground/case)
    • There is a breakdown of the motor or motor wiring insulation (You would probably need to use a 1000-Volt megger to check for an insulation breakdown)
    • There could also be a problem with one or more of the LEM modules on the drive

31JAN2023 jd

  • DESAT
  • OVER I
  • fault
  • OVERCURRENT
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply