Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base INTCAP
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base INTCAP
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
INTCAP

Print Friendly and PDF

 

Products: ACR9000, 9030,9040,9600,9630,9640

Supplement to INTCAP command in ACR Command Language Reference.

Capture Register: Specifies which register is armed to hold the captured position.
If the hardware capture register is not specified, the hardware capture register index is the same as the feedback encoder index of the axis used to enable the hardware capture. The capture complete flag and hardware capture parameter for the encoder capture is selected based on the axis used to enable the hardware capture.

In this example,  ENC1 is attached to AXIS1, therefore the default Capture Register is 1
 
AXIS1 INTCAP 2
REM Rising First External -- Inp 25
REM Hardware Capture Parameter -- P12548
REM Capture Complete Flag -- BIT809

If the hardware capture register is specified then the capture parameter must also be specified. The capture complete flags and hardware capture parameters are still in pairs, but are not based on the axis used to enable the hardware capture.
AXIS1 INTCAP 10 CAP3 P13060
REM Rising Third External -- Inp 25
REM Hardware Capture Parameter -- P13060
REM Capture Complete Flag -- BIT873
 
Table Key
MRK= Encoder Z Mark
INP=Digital Input
+  = Rising Edge
- = Falling Edge

SRC ENC0,1,2,3,8 ENC4,5,6,7,9 EPLD
Aries-PE Compax3
capture_ register 0 1 2 3 4 5 6 7 0 0
Mode                    
0 +MRK 0 +MRK 1 +MRK 2 +MRK 3 +MRK 4 +MRK 5 +MRK 6 +MRK 7 +MRK 0  
1 +MRK 1 +MRK 0 +MRK 3 +MRK 2 +MRK 5 +MRK 4 +MRK 7 +MRK 6    
2 +INP 24 +INP 25 +INP 26 +INP 27 +INP 72 +INP 73 +INP 74 +INP 75 +INP 5 +INP 0
3 +INP 25 +INP 24 +INP 27 +INP 26 +INP 73 +INP 72 +INP 75 +INP 74 +INP 6 +INP 1
4 -MRK 0 -MRK 1 -MRK 2 -MRK 3 -MRK 4 -MRK 5 -MRK 6 -MRK 7 -MRK 0  
5 -MRK 1 -MRK 0 -MRK 3 -MRK 2 -MRK 5 -MRK 4 -MRK 7 -MRK 6    
6 -INP 24 -INP 25 -INP 26 -INP 27 -INP 72 -INP 73 -INP 74 -INP 75 -INP 5 -INP 0
7 -INP 25 -INP 24 -INP 27 -INP 26 -INP 73 -INP 72 -INP 75 -INP 74 -INP 6 -INP 1
8 +MRK 2 +MRK 3 +MRK 0 +MRK 1 +MRK 6 +MRK 7 +MRK 4 +MRK 5    
9 +MRK 3 +MRK 2 +MRK 1 +MRK 0 +MRK 7 +MRK 6 +MRK 5 +MRK 4    
10 +INP 26 +INP 27 +INP 24 +INP 25 +INP 74 +INP 75 +INP 72 +INP 73 +INP 4 +INP 2
11 +INP 27 +INP 26 +INP 25 +INP 24 +INP 75 +INP 74 +INP 73 +INP 72   +INP 3
12 -MRK 2 -MRK 3 -MRK 0 -MRK 1 -MRK 6 -MRK 7 -MRK 4 -MRK 5    
13 -MRK 3 -MRK 2 -MRK 1 -MRK 0 -MRK 7 -MRK 6 -MRK 5 -MRK 4    
14 -INP 26 -INP 27 -INP 24 -INP 25 -INP 74 -INP 75 -INP 72 -INP 73 -INP 4 -INP 2
15 -INP 27 -INP 26 -INP 25 -INP 24 -INP 75 -INP 74 -INP 73 -INP 72   -INP 3
16 +MRK 8 +MRK 8 +MRK 8 +MRK 8 +MRK 9 +MRK 9 +MRK 9 +MRK 9    
18 +INP 28 +INP 29 +INP 30 +INP 31 +INP 76 +INP 77 +INP 78 +INP 79   +INP 4
19 +INP 29 +INP 28 +INP 31 +INP 30 +INP 77 +INP 76 +INP 79 +INP 78   +INP 5
20 -MRK 8 -MRK 8 -MRK 8 -MRK 8 -MRK 9 -MRK 9 -MRK 9 -MRK 9    
22 -INP 28 -INP 29 -INP 30 -INP 31 -INP 76 -INP 77 -INP 78 -INP 79   -INP 4
23 -INP 29 -INP 28 -INP 31 -INP 30 -INP 77 -INP 76 -INP 79 -INP 78   -INP 5
26 +INP 30 +INP 31 +INP 28 +INP 29 +INP 78 +INP 79 +INP 76 +INP 77   +INP 6
27 +INP 31 +INP 30 +INP 29 +INP 28 +INP 79 +INP 78 +INP 77 +INP 76   +INP 7
30 -INP 30 -INP 31 -INP 28 -INP 29 -INP 78 -INP 79 -INP 76 -INP 77   -INP 6
31 -INP 31 -INP 30 -INP 29 -INP 28 -INP 79 -INP 78 -INP 77 -INP 76   -INP 7

 

 

Axis Capture Complete Flag Hardware Capture Position
0 777 12292
1 809 12548
2 841 12804
3 873 13060
4 905 13316
5 937 13572
6 969 13828
7 1001 14084
8 7689 14340
9 7721 14596
10 7753 14852
11 7785 15108
12 7817 15364
13 7849 15620
14 7881 15876
15 7913 16132

 

 

jw updated 07-Dec-2012