Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base TASX Bit 28 -- Motor Configuration Warning
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base TASX Bit 28 -- Motor Configuration Warning
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)-
      • 24 Volt Keep Alive
      • Analog input on GV6, GV6K, GT6, GT6K
      • Audible Noise in Stepper Motors
      • Cable breakout modules for the Gemini
      • Can I run the MX80L using a Gemini Drive?
      • Can the Gemini Products take a DC voltage supply?
      • Changing Motor direction on the GV6 or GT6
      • Chopping frequency of the Gemini drive.
      • Connector Part Numbers
      • Controller to GV Cables
      • Currently Released Gemini Drive Products
      • Daisy chaining GVs and GTs
      • Digital Notch Filters
      • Does the Gemini drive have a test mode?
      • Downloading the OS to my Gem6K locks up.
      • Encoder Motors Work with Gemini Resolver units
      • ERES /ORES Relationship for Gemini GV Products
      • GC-SDA Fault output is not really the fault output
      • GEM-VM50 screw-terminal breakout dimensions
      • Gem6K (GV6K & GT6K) Family Letter of Volatility
      • Gemini MaxPlus (MPM) Resolver Option 1 Connection
      • Gemini - Downloading in
      • Gemini - MaxPlus (MPM) Encoder Option 1 Connection
      • Gemini - MaxPlus (MPM) Encoder Option 5 Connection
      • Gemini Analog Input Deadband
      • Gemini Analog Output A now dithers
      • Gemini GV - Resolver to Encoder Signal Conversion
      • Gemini GV6 & GT6 RS232 Daisy-Chaining ERRLVL
      • Gemini Maximum Frequency Input and Output
      • Gemini OS Download Failures
      • Gemini Step & Direction Inputs
      • Gemini Update Rates.
      • Gemini Variable Resolution
      • Gemini: 400LXR Tuning
      • Gemini: ASCII or Binary?
      • Gemini: VIDEO: express basics training: How to Connect Ethernet (includes Win7)
      • Getting the letter a with a ~ over it in Motion Planner Terminal
      • GFB-KIT Pinout
      • GV Cable Diameters.
      • GV6K & GT6K cannot Follow Analog Onboard Input
      • GV6K Tuning in Position Mode with Motion Planner
      • Hall State Checking on Gemini Products
      • Hall-less Startup on Gemini
      • I cannot communicate with my GEM-6K.
      • Limits on Gemini
      • MS cable option vs. GS cable option
      • OS 1.70 Additions
      • Replacing the Gemini GC-SDA
      • RESET command in STARTP program
      • Resolution of the Gemini command signal.
      • RS232 Troubleshooting for the Geminis
      • Step & Direction Output
      • TASX Bit 1 -- Motor Temperature Fault
      • TASX Bit 10 - Bridge Fault (Hardware)
      • TASX Bit 11 -- Bridge Over-Temp Fault (Software)
      • TASX Bit 12 -- Over-Voltage Fault
      • TASX Bit 17 -- Stall Detected
      • TASX Bit 18 -- Override mode
      • TASX Bit 19 -- Foldback Active
      • TASX Bit 2 -- Low Voltage Fault
      • TASX Bit 20 -- Power Dissipation Circuit Active
      • TASX Bit 21 -- Bad Hall State Detected
      • TASX Bit 22 -- Unrecognized Hardware Detected
      • TASX Bit 23 -- User Fault Input Active
      • TASX Bit 24 -- Keep Alive Circuit Active
      • TASX Bit 25 -- Power Dissipation Circuit Fault
      • TASX Bit 28 -- Motor Configuration Warning
      • TASX Bit 29 -- ORES Failure
      • TASX Bit 3 -- Drive Temperature Fault
      • TASX Bit 30 -- Motor Thermal Model
      • TASX Bit 31 -- Commanded Torque Limit Hit
      • TASX Bit 5 -- Encoder/Resolver Failed
      • TASX Bit 7 -- Motor Configuration Error
      • TASX Bit 8 -- Incoming Pulses
      • TASX Bit 9 -- Velocity Error Limit Exceeded
      • The GV and Linear Motors
      • Tuning a GV6K GV6 or GV in Position Mode
      • Tuning GV or GV6 drives with large inertia loads.
      • Tuning the Gemini in Position Mode
      • Tuning the Gemini in Position Mode.
      • Tuning the Gemini in Torque Mode.
      • Tuning the Gemini in Velocity Mode.
      • Using Gemini with Empire Magnetics Step Motors
      • VIDEO: Basics Training: GV or GT drives
      • VIDEO: Basics training: GV6 or GT6 drive controllers
      • VIDEO: Basics training: GV6K or GT6K drive controllers
      • What are Q and D currents?
      • What does the Error Log contain?
      • What drives can work with a DC brushed motor?
      • What happens in Keep Alive mode?
      • What motors with what Gemini drive?
      • What recognitions does the Gemini GV have?
      • What replaces the Gemini GT stepper drive?
      • What replaces the Gemini GT6 stepper drive/controller?
      • What replaces the Gemini GT6K stepper drive/controller?
      • What replaces the Gemini GV6K servo drive controller?
      • Which Motors Work with GV-L Drives? GV-U Drives?
      • Which rotation is considered positive for GV6K?
      • Why doesn't my Drive I/O cable tighten down securely when using the jackscrews?
      • Why will my PAD and PED not update on the Gemini?
      • Z channel output from the Gemini?
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
TASX Bit 28 -- Motor Configuration Warning

Print Friendly and PDF
This bit occurs when a “mismatch” has been detected between a Gemini drive and the motor configured to be used with it. As an example, when the requirements for a motor far exceed the particular Gemini drive’s ability to fulfill those requirements (say, a GV-U3 with a M1053K motor), this bit will activate with a TCS 400 -- or similar -- warning code. A TCS code indicates a configuration parameter that has been flagged due to a non-ideal value or motor/drive combination. However, this is only a warning bit, and will not interfere with motor operation.

REMEDY:

Use the TCS command to determine the specific cause of the warning, then correct or modify the appropriate parameter(s) as necessary.
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply