Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base TASX Bit 1 -- Motor Temperature Fault
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base TASX Bit 1 -- Motor Temperature Fault
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)-
      • 24 Volt Keep Alive
      • Analog input on GV6, GV6K, GT6, GT6K
      • Audible Noise in Stepper Motors
      • Cable breakout modules for the Gemini
      • Can I run the MX80L using a Gemini Drive?
      • Can the Gemini Products take a DC voltage supply?
      • Changing Motor direction on the GV6 or GT6
      • Chopping frequency of the Gemini drive.
      • Connector Part Numbers
      • Controller to GV Cables
      • Currently Released Gemini Drive Products
      • Daisy chaining GVs and GTs
      • Digital Notch Filters
      • Does the Gemini drive have a test mode?
      • Downloading the OS to my Gem6K locks up.
      • Encoder Motors Work with Gemini Resolver units
      • ERES /ORES Relationship for Gemini GV Products
      • GC-SDA Fault output is not really the fault output
      • GEM-VM50 screw-terminal breakout dimensions
      • Gem6K (GV6K & GT6K) Family Letter of Volatility
      • Gemini MaxPlus (MPM) Resolver Option 1 Connection
      • Gemini - Downloading in
      • Gemini - MaxPlus (MPM) Encoder Option 1 Connection
      • Gemini - MaxPlus (MPM) Encoder Option 5 Connection
      • Gemini Analog Input Deadband
      • Gemini Analog Output A now dithers
      • Gemini GV - Resolver to Encoder Signal Conversion
      • Gemini GV6 & GT6 RS232 Daisy-Chaining ERRLVL
      • Gemini Maximum Frequency Input and Output
      • Gemini OS Download Failures
      • Gemini Step & Direction Inputs
      • Gemini Update Rates.
      • Gemini Variable Resolution
      • Gemini: 400LXR Tuning
      • Gemini: ASCII or Binary?
      • Gemini: VIDEO: express basics training: How to Connect Ethernet (includes Win7)
      • Getting the letter a with a ~ over it in Motion Planner Terminal
      • GFB-KIT Pinout
      • GV Cable Diameters.
      • GV6K & GT6K cannot Follow Analog Onboard Input
      • GV6K Tuning in Position Mode with Motion Planner
      • Hall State Checking on Gemini Products
      • Hall-less Startup on Gemini
      • I cannot communicate with my GEM-6K.
      • Limits on Gemini
      • MS cable option vs. GS cable option
      • OS 1.70 Additions
      • Replacing the Gemini GC-SDA
      • RESET command in STARTP program
      • Resolution of the Gemini command signal.
      • RS232 Troubleshooting for the Geminis
      • Step & Direction Output
      • TASX Bit 1 -- Motor Temperature Fault
      • TASX Bit 10 - Bridge Fault (Hardware)
      • TASX Bit 11 -- Bridge Over-Temp Fault (Software)
      • TASX Bit 12 -- Over-Voltage Fault
      • TASX Bit 17 -- Stall Detected
      • TASX Bit 18 -- Override mode
      • TASX Bit 19 -- Foldback Active
      • TASX Bit 2 -- Low Voltage Fault
      • TASX Bit 20 -- Power Dissipation Circuit Active
      • TASX Bit 21 -- Bad Hall State Detected
      • TASX Bit 22 -- Unrecognized Hardware Detected
      • TASX Bit 23 -- User Fault Input Active
      • TASX Bit 24 -- Keep Alive Circuit Active
      • TASX Bit 25 -- Power Dissipation Circuit Fault
      • TASX Bit 28 -- Motor Configuration Warning
      • TASX Bit 29 -- ORES Failure
      • TASX Bit 3 -- Drive Temperature Fault
      • TASX Bit 30 -- Motor Thermal Model
      • TASX Bit 31 -- Commanded Torque Limit Hit
      • TASX Bit 5 -- Encoder/Resolver Failed
      • TASX Bit 7 -- Motor Configuration Error
      • TASX Bit 8 -- Incoming Pulses
      • TASX Bit 9 -- Velocity Error Limit Exceeded
      • The GV and Linear Motors
      • Tuning a GV6K GV6 or GV in Position Mode
      • Tuning GV or GV6 drives with large inertia loads.
      • Tuning the Gemini in Position Mode
      • Tuning the Gemini in Position Mode.
      • Tuning the Gemini in Torque Mode.
      • Tuning the Gemini in Velocity Mode.
      • Using Gemini with Empire Magnetics Step Motors
      • VIDEO: Basics Training: GV or GT drives
      • VIDEO: Basics training: GV6 or GT6 drive controllers
      • VIDEO: Basics training: GV6K or GT6K drive controllers
      • What are Q and D currents?
      • What does the Error Log contain?
      • What drives can work with a DC brushed motor?
      • What happens in Keep Alive mode?
      • What motors with what Gemini drive?
      • What recognitions does the Gemini GV have?
      • What replaces the Gemini GT stepper drive?
      • What replaces the Gemini GT6 stepper drive/controller?
      • What replaces the Gemini GT6K stepper drive/controller?
      • What replaces the Gemini GV6K servo drive controller?
      • Which Motors Work with GV-L Drives? GV-U Drives?
      • Which rotation is considered positive for GV6K?
      • Why doesn't my Drive I/O cable tighten down securely when using the jackscrews?
      • Why will my PAD and PED not update on the Gemini?
      • Z channel output from the Gemini?
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
TASX Bit 1 -- Motor Temperature Fault

Print Friendly and PDF
This error is the result of an open thermal switch circuit between the motor and the Gemini drive.

When the motor's internal thermal switch gets to a certain temperature, typically around 125 degrees C, it opens thereby telling the drive that it is hot. The case temperature of the motor becoming extremely hot often accompanies this condition.

This can also be attributed to a broken, loose, disconnected or missing thermal switch wire between the drive and motor.

REMEDIES:

1) Check the thermal wire connections between the drive
and motor to insure that they are securely connected. If all connections are secure, disconnect the feedback cable from the Gemini and measure the resistance between
the two thermal wires in the cable with an ohmmeter. If a large resistance is measured, the thermal switch is bad, and the motor will need to be sent in for repair. A good temperature switch will measure much less than 1 ohm.

2) If using Gemini Operating System 1.83 or newer, the DTHERM1 command can be used to disable thermal switch-checking altogether. (NOTE: The DTHERM1 command is REQUIRED when using BE16 motors with the Gemini, as these motors have no thermal switch.)

3) Make sure that you are using the correct cables between the Gemini and motor. Also make sure the motor's connection-type is compatible with the cables and Gemini. For example, the difference between the SM motors with the -MS and -GS type connections is that the thermal wires were moved from the motor cable in the -MS to the feedback cable in the -GS. Other than that change, the cables are the same. Therefore, a Gemini using the SM's GS CABLE kits with an SM motor that has the -MS connections will cause the thermal switch to be seen as open.
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply